Write-Read |
About Internal DC Sources |
Description |
Sets the X-axis of the selected measurement to a DC Source. This command does not change the default setting for new traces. |
VB Syntax |
Meas.XAxisSource= value |
Variable |
(Type) - Description |
Meas |
A Measurement (object) |
value |
(String) - Not case-sensitive. For all channels EXCEPT DIQ, choose from the following: "Default" - The default X-axis setting for the selected measurement. For Application measurements, the X-Axis domain is set with specific commands. "AO1" - Internal DC source #1 "AO2" - Internal DC source #2 Note: For DIQ channels, see XAxisDomain Property |
Example |
Meas.XAxis = "Default" 'Write value = Meas.XAxis 'Read |
C++ Syntax |
HRESULT put_XAxis(BSTR source); HRESULT get_XAxis(BSTR* source); |
Interface |
IMeasurement17 |