ABORt
Applicable Models: All (Write-only) Stops all sweeps - then resume per current trigger settings. This command is the same as INITtiate:IMMediate (restart) except if a channel is performing a single sweep, ABORt will stop the sweep, but not initiate another sweep. Learn about Synchronizing the Analyzer and Controller |
|
Examples |
ABOR |
Query Syntax |
Not applicable |
Default |
Not applicable |