| CALCulate:MEASure:FUNCtion DOMain | USER | [:RANGe] | STARt | STOP STATistics | [:STATe] | 
Click a keyword to view the command details.
See Also
| Applicable Models: All (Read-only) Returns the trace statistic data for the selected statistic type for the specified channel. Select the type of statistic with CALC:MEAS:FUNC:TYPE. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| Return Type | Depends on FORM:DATA | 
| Example | 
 | 
| Not applicable | |
| Applicable Models: All (Read-Write) Sets the range used to calculate trace statistics. Each channel has 16 user ranges. The x-axis range is specified with the CALC:MEAS:FUNC:DOM:USER:START and STOP commands. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <range> | Range number. Choose from: 0 to 16 0 is Full Span of the current x-axis range 1 to 16 are user-specified ranges | 
| Examples | CALC:MEAS2:FUNC:DOM:USER 
		 4 | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:FUNCtion:DOMain:USER[:RANGe]? | 
| Return Type | Numeric | 
| 0 - Full Span | |
| Applicable Models: All (Read-Write) Sets the start of the specified user-domain range. To apply this range, use CALC:MEAS:FUNC:DOM:USER To set the stop of the range, use CALC:MEAS:FUNC:DOM:USER:STOP. Note: This command does the same as CALC:MEAS:MARK:FUNC:DOM:USER:STAR | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <range> | Range number that will receive the start value. Choose an integer between 1 and 16 | 
| <start> | Start value of the specified range. 
		 Choose a real number between: | 
| Examples | CALC:MEAS2:FUNC:DOM:USER:STAR 
		 1,1e9 | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:FUNCtion:DOMain:USER:STARt? <range> | 
| Return Type | Numeric | 
| The analyzer's Minimum x-axis value | |
| Applicable Models: All (Read-Write) Sets the stop value of the specified user-domain range. To apply this range, use CALC:MEAS:FUNC:DOM:USER. To set the start of the range, use CALC:MEAS:MARK:FUNC:DOM:USER:STAR Note: This command does the same as CALC:MEAS:MARK:FUNC:DOM:USER:STOP | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <range> | Range number that will receive the stop value. Choose an integer between 1 and 16 | 
| <stop> | Stop value of the specified range. 
		 Choose a real number between: | 
| Examples | CALC:MEAS2:FUNC:DOM:USER:STOP 
		 4,5e9 | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:FUNCtion:DOMain:USER:STOP? <range> | 
| Return Type | Numeric | 
| The analyzer's Maximum x-axis value | |
| Applicable Models: All (Write-only) For the active trace of specified channel, executes the statistical analysis specified by the CALC:MEAS:FUNC:TYPE command. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| Examples | CALC:MEAS2:FUNC:EXEC | 
| Query Syntax | Not Applicable | 
| Not Applicable | |
| Applicable Models: All (Read-Write) Displays and hides the trace statistics (peak-to-peak, mean, standard deviation) on the screen. The analyzer will display either measurement statistics or Filter Bandwidth statistics; not both. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <ON|OFF> | ON - Displays trace statistics OFF - Hides trace statistics | 
| Examples | CALC:MEAS2:FUNC:STAT 
		 ON | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:FUNCtion:STATistics[:STATe]? | 
| Return Type | Boolean (1 = ON, 0 = OFF) | 
| OFF (0) | |
| Applicable Models: All (Read-Write) For Smith Chart format, changes trace statistics (peak-to-peak, mean, standard deviation) units from Log Mag (dB) to impedance (ohms) on the screen. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <ON|OFF> | ON - Units displayed in ohms OFF - Units displayed in dB | 
| Examples | CALC:MEAS2:FUNC:STAT:RES ON | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:FUNCtion:STATistics:RESistance[:STATe]? | 
| Return Type | Boolean (1 = ON, 0 = OFF) | 
| OFF (0) | |
| Applicable Models: All (Read-Write) Sets statistic TYPE that you can then query using CALC:MEAS:FUNCtion:DATA?. Note: This command affects only the selected measurement on the specified channel. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <char> | Choose from: PTPeak - the difference between the max and min data points on the trace. STDEV - standard deviation of all data points on the trace MEAN - mean (average) of all data points on the trace MIN - lowest data point on the trace MAX - highest data point on the trace | 
| Examples | CALC:MEAS2:FUNC:TYPE 
		 PTP | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:FUNCtion:TYPE? | 
| Return Type | Character | 
| PTPeak | |