CALCulate:MEASure:GDELay Commands

Controls the Aperture setting used to make Group Delay measurements.

CALCulate:MEASure:GDELay

FREQuency

PERCent

POINts

Click a keyword to view the command details.

See Also


CALCulate<cnum>:MEASure<mnum>:GDELay:FREQuency <value>

Applicable Models: All

(Read-Write) Sets group delay aperture using a fixed frequency range.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<value>

Frequency range (in Hz) to use for the aperture setting. Choose between the equivalent of two data points and the channel frequency span.

Examples

CALC:MEAS2:GDEL:FREQ 1E6

Query Syntax

CALCulate<cnum>:MEASure<mnum>:GDELay:FREQuency?

Return Type

Numeric

Default

Frequency range that equates to 11 points. This can be changed to two points with a preference setting.


CALCulate<cnum>:MEASure<mnum>:GDELay:PERCent <value>

Applicable Models: All

(Read-Write) Sets group delay aperture using a percent of the channel frequency span.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<value>

Percent of frequency span to use for the aperture setting. Choose between the equivalent of two data points and 100 percent of the channel frequency span.

Examples

'set to 25 percent of the channel frequency span

CALC:MEAS2:GDEL:PERC 25

Query Syntax

CALCulate<cnum>:MEASure<mnum>:GDELay:PERCent?

Return Type

Numeric

Default

Percent of frequency span that equates to 11 points. This can be changed to two points with a preference setting.


CALCulate<cnum>:MEASure<mnum>:GDELay:POINts <value>

Applicable Models: All

(Read-Write) Sets group delay aperture using a fixed number of data points.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<value>

Number of data points to  use for the aperture setting. Choose between two points and the number of points in the channel.

Examples

'set to 25 data points

CALC:MEAS2:GDEL:POIN 25

Query Syntax

CALCulate<cnum>:MEASure<mnum>:GDELay:POINts?

Return Type

Numeric

Default

11 points. This can be changed to two points with a preference setting.