Controls the limit segments used for pass / fail testing.
| CALCulate:MEASure:LIMit | DELete DISPlay | [:STATe] REPort | ALL? | [:DATA]? | POINts? SEGMent | AMPLitude | STARt | STOP | COUNt? | STIMulus | STARt | STOP | TYPE SOUNd | [:STATe] | 
Click a keyword to view the command details.
See Also
| Applicable Models: All (Read-Write) Sets data for limit segments. | |||||||||||
| Parameters | 
 | ||||||||||
| <cnum> | Channel number of the measurement (optional). | ||||||||||
| <mnum> | Measurement number for each measurement. | ||||||||||
| <block> | Data 
		 for all limit segments. The following is the data format for 1 
		 segment: 
 | ||||||||||
| Examples | The following writes three max limit segments for a bandpass filter. CALC:MEAS2:LIM:DATA 1,3e5,4e9,-60,0,1,4e9,7.5e9,0,0,1,7.5e9,9e9,0,-30 | ||||||||||
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:LIMit:DATA? | ||||||||||
| Return Type | Depends on FORM:DATA | ||||||||||
| Maximum limit = 100 | |||||||||||
| Applicable Models: All (Write-only) Deletes all limit line data for the selected measurement on the specified channel. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| Examples | CALC2:MEAS2:LIM:DATA:DEL | 
| Query Syntax | Not Applicable | 
| Not Applicable | |
| Applicable Models: All (Read-Write) Turns the display of limit segments ON or OFF (if the data trace is turned ON). | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <ON | OFF> | ON 
		 (or 1) - turns the display 
		 of limit segments ON. | 
| Examples | CALC:MEAS2:LIM:DISP:STAT 
		 ON | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:LIMit:DISPlay[:STATe]? | 
| Return Type | Boolean (1 = ON, 0 = OFF) | 
| ON | |
| Applicable Models: All (Read-only) Returns the Pass / Fail status of the limit line test. Returns 1 (Fail) if any data point fails for any limit segment. Limit display (CALC:LIM:DISP) does NOT have to be ON. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| Examples | CALC:MEAS2LIM:FAIL? | 
| Return Type | Boolean 
 | 
| Not Applicable | |
| Applicable Models: All (Read-only) Returns the test results (stimulus value, limit test result, upper limit value and lower limit value of all measurement points), for the selected trace. This command returns a point by point description of the limit table and pass/fail test result. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <block> | Depends on FORM:DATA If the number of the measurement points is N, <Block> = <first stimulus>,<test result>,<upper limit>,<lower limit>, …, <Nth stimulus>,<test result>,<upper limit>,<lower limit> Where <test result>= -1: No limit, 0:Fail, 1:Pass | 
| Examples | The following example returns three points: CALC:MEAS2:LIM:REP:ALL? +1.00000000000E+009, 'bucket 1 XAxis value +1.00000000000E+000, 'result (1 == Pass) -4.90000009537E+000, 'upper limit -5.05000019073E+000, 'lower limit 
 +3.00000000000E+009, 'bucket 2 XAxis value +1.00000000000E+000, -4.84999990463E+000, -5.19999980927E+000, 
 +5.00000000000E+009, 'bucket 3 Xaxis value -1.00000000000E+000, +0.00000000000E+000, +0.00000000000E+000 | 
| Return Type | Variant | 
| Depend on the preset status | |
| Applicable Models: All (Read-only) Returns the stimulus values (frequency, power level or time) at all the measurement points that failed the limit test, for the selected trace. If there are no failures, a large number is returned (+9.91000000000E+037). | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <block> | Depends on FORM:DATA If the number of the measurement points that failed the limit test is N, <block>=<First failed stimulus>, ..., <Nth failed stimulus>. | 
| Examples | The following example assumes that there are no failures: CALC:MEAS2:LIM:REP:DATA? +9.91000000000E+037 | 
| Return Type | Numeric | 
| 9.91E37 (no failures) | |
| Applicable Models: All (Read-only) Reads the number of the measurement points that failed the limit test, for the active trace of selected channel. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| Examples | CALC:MEAS:LIM:REP:POIN? | 
| Query Syntax | Numeric | 
| 0 | |
| Applicable Models: All (Read-Write) Sets the start (beginning) of the Y-axis amplitude (response) value. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <snum> | Segment number; if unspecified, value is set to 1. | 
| <num> | Choose any number between: -500 and 500 Display value is limited to the Maximum and Minimum displayed Y-axis values. | 
| Examples | CALC:MEAS2LIM:SEGM1:AMPL:STAR 
		 10 | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>AMPLitude:STARt? | 
| Return Type | Numeric | 
| 0 | |
| Applicable Models: All (Read-Write) Sets the stop (end) of the Y-axis amplitude (response) value. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <snum> | Segment number; if unspecified, value is set to 1. | 
| <num> | Choose any number between: -500 and 500 Display value is limited to the Maximum and Minimum displayed Y-axis values. | 
| Examples | CALC:MEAS:LIM:SEGM1:AMPL:STOP 
		 10 | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>AMPLitude:STOP? | 
| Return Type | Numeric | 
| 0 | |
| Applicable Models: All (Read-only) Returns the number of segments used in a limit test. All segments are counted, whether they are on or not. | |
| Parameters | Not Applicable | 
| <mnum> | Measurement number for each measurement. | 
| Examples | CALC:MEAS2:LIM:SEGM:COUN? | 
| Return Type | Numeric | 
| Not Applicable | |
| Applicable Models: All (Read-Write) Sets the start (beginning) of the X-axis stimulus value. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <snum> | Segment number; if unspecified, value is set to 1. | 
| <num> | Choose any number within the X-axis span of the analyzer. | 
| Examples | CALC:MEAS:LIM:SEGM1:STIM:STAR 
		 10 | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>STIMulus:STARt? | 
| Return Type | Numeric | 
| 0 | |
| Applicable Models: All (Read-Write) Sets the stop (end) of the X-axis stimulus value. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <snum> | Segment number; if unspecified, value is set to 1. | 
| <num> | Choose any number within the X-axis span of the analyzer. | 
| Examples | CALC:MEAS2:LIM:SEGM1:AMPL:STOP 
		 10 | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>STIMulus:STOP? | 
| Return Type | Numeric | 
| 0 | |
| Applicable Models: All (Read-Write) Sets the type of limit segment. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <snum> | Segment 
		 number. Choose any number between: | 
| <char> | Choose from: LMIN - a MIN limit segment. Any response data below the MIN value will fail. OFF - the limit segment (display and testing) is turned OFF. | 
| Examples | CALC:MEAS2:LIM:SEGM:TYPE 
		 LMIN | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>:TYPE? | 
| Return Type | Character | 
| OFF | |
| Applicable Models: All (Read-Write) Turns limit testing fail sound ON or OFF. | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <ON | OFF> | ON 
		 (or 1) - turns sound ON. | 
| Examples | CALC:MEAS2:LIM:SOUN 
		 ON | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:LIMit:SOUNd[:STATe]? | 
| Return Type | Boolean (1 = ON, 0 = OFF) | 
| OFF | |
| Applicable Models: All (Read-Write) Turns limit segment testing ON or OFF. 
 | |
| Parameters | 
 | 
| <cnum> | Channel number of the measurement (optional). | 
| <mnum> | Measurement number for each measurement. | 
| <ON | OFF> | ON 
		 (or 1) - turns limit testing 
		 ON. | 
| Examples | CALC:MEAS:LIM:STAT 
		 ON | 
| Query Syntax | CALCulate<cnum>:MEASure<mnum>:LIMit:STATe? | 
| Return Type | Boolean (1 = ON, 0 = OFF) | 
| OFF | |