This command is Superseded by the CALCulate:MEASure:MIXer:XAXis command.
CALCulate<ch>:MIXer:XAXis <char>
| Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Sets or returns the swept parameter to display on the X-axis for the selected FCA and GCX measurement. Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more. | |
| Parameters | 
 | 
| <ch> | Any existing channel number. If unspecified, value is set to 1. | 
| <char> | Parameter to display on the X-axis. Choose from: INPUT - Input frequency span OUTPUT - Output frequency span LO_1 - First LO frequency span LO_2 - Second LO frequency span | 
| Examples | CALC:MIX:XAX 
		 INPUT See an example that creates, selects, and calibrates an SMC and VMC measurement using SCPI. | 
| Query Syntax | CALCulate<ch>:MIXer:XAXis? | 
| Return Type | Character | 
| OUTPUT | |