CALulate:TDR Commands

These commands control the setup and execution of TDR measurements.

CALCulate:TDR

ALLocate

DEEM

    | BPOT:FILename

    | BPOR:STATe

    | LENGth

    | PORT:FILename

    | PORT:STATe

    | STATe

DEVice

EMPHasis

     | CURSor

          | POST1

          | POST2

          | PRE1

     | STATe

EQUalization

     | CTLE

          | DC

          | POLE1

          | POLE2

          | ZERO1

     | FILename

     | STATe

     | TYPE

EYE

     | EXECute

     | INPut

          | BPATtern

                | LENGth

                | TYPE

          | DRATe

          | JITTer

                | DLIMit

                | PERiodic

                      | FREQuency

                      | MAGNitude

                | RANDom

                      | MAGNitude

                | STATe

                | TYPE

          | OLEVel

          | RTIMe

                | DATA

                | THReshold

          | ZLEVel

     | MASK

          | FAIL?

          | STATe

     | RESults

          | DATA?

          | DISPlay

                | STATe

          | THReshold

     | STATe

MEASure

     | ACTive

          | MARKer

     | DTIMe

          | DATA?

          | POSition

          | STATe

          | TARGet

     | FORMat

     | MARKer

           | REFerence

                | STATe

           | STATe

     | PARameter

     | PEELing

          | STATe

     | SMOothing

          | STATe

     | TIME

          | COUPle

          | IMPulse

               | WIDTh

          | STEP

               | RTIMe

                     | THReshold

               | COUPle

          | TYPE

     | TTIMe

          | DATA

          | STATe

          | THReshold

TIME

    | STEP

         | AMPLitude

 

Click on a red keyword to view the command details.

See Also


CALCulate<cnum>:TDR:ALLocate <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the type of parameter and format allocation for each trace.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Parameters to display. Choose from:

SPARameters - Display all S-parameter data.

TPARameters - Display all Time domain data.

MIXed - Display a mix of commonly measured time-domain and S-parameter data.

Examples

CALC:TDR:ALL SPAR
calculate2:tdr:allocate sparameters

Query Syntax

CALCulate<cnum>:TDR:ALLocate?

Return Type

String

Default

MIXed


CALCulate<cnum>:TDR:DEVice <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the DUT topology.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Topology. Choose from:

SEND1 - Single-ended, 1-port.

SEND2 - Single-ended, 2-port.

DIF1 - Differential, 1-port.

SEND4 - Single-ended, 4-port.

DIF2 - Differential, 2-port.

Examples

CALC:TDR:DEV SEND2
calculate2:tdr:device:send2

Query Syntax

CALCulate<cnum>:TDR:DEVice?

Return Type

String

Default

SEND1

 


CALCulate<cnum>:TDR:DEEM:BPOR<pnum>:FILename <file> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the filename of the s4p de-embedding user file.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<pnum>

Port number for balance port.  If unspecified, <pnum> is set to 1.

<file>

File Name. This file is saved as a 4-port touchstone file with the .s4p extensions.

Examples

CALC:TDR:DEEM:BPOR1:FIL "test.s4p"
calculate2:tdr:deem:bport2:filename "test.s4p"

Query Syntax

CALCulate<cnum>:TDR:DEEM:BPOR<pnum>:FILename?

Return Type

String

Default

" " (Empty String)


CALCulate<cnum>:TDR:DEEM:BPOR<pnum>:STATe <bool> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets s4p de-embedding function state ON/OFF.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<pnum>

Port number for balance port.  If unspecified, <pnum> is set to 1.

<bool>

ON or 1 - Turns s4p de-embedding function ON.
OFF or 0
- Turns s4p de-embedding function OFF.

Examples

CALC:TDR:DEEM:BPOR1:STAT ON
calculate2:tdr:deem:bport2:state off

Query Syntax

CALCulate<cnum>:TDR:DEEM:BPOR<pnum>:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:DEEM:LENGth

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the approximate fixture length

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Approximate fixture length (range: 0 to max DUT length)

Examples

CALC:TDR:DEEM:LENG 1.5e-9
calculate2:tdr:deem:length 1.3e-9

Query Syntax

CALCulate<cnum>:TDR:DEEM:LENGth?

Return Type

Double

Default

0


CALCulate<cnum>:TDR:DEEM:PORT<pnum>:FILename <file> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the filename of the s2p de-embedding user file.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<pnum>

Port number.  If unspecified, <pnum> is set to 1.

<file>

File Name. This file is saved as a 2-port touchstone file with the .s2p extensions.

Examples

CALC:TDR:DEEM:PORT1:FIL "test.s2p"
calculate2:tdr:deem:port2:filename "test.s2p"

Query Syntax

CALCulate<cnum>:TDR:DEEM:PORT<pnum>:FILename?

Return Type

String

Default

" " (Empty String)


CALCulate<cnum>:TDR:DEEM:PORT<pnum>:STATe <bool> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets s2p de-embedding function state ON/OFF.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<pnum>

Port number.  If unspecified, <pnum> is set to 1.

<bool>

ON or 1 - Turns s2p de-embedding function ON.
OFF or 0
- Turns s2p de-embedding function OFF.

Examples

CALC:TDR:DEEM:PORT1:STAT ON
calculate2:tdr:deem:port2:state off

Query Syntax

CALCulate<cnum>:TDR:DEEM:PORT<pnum>:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:DEEM:STATe <bool> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets de-embedding function state ON/OFF.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns  de-embedding function ON.
OFF or 0
- Turns de-embedding function OFF.

Examples

CALC:TDR:DEEM:STAT ON
calculate2:tdr:deem:state off

Query Syntax

CALCulate<cnum>:TDR:DEEM::STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:EMPHasis:CURSor:POST1 <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the emphasis post1 level.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Post1 level value. The range is -20 dB to +20 dB.

Examples

CALC:TDR:EMPH:CURS:POST1 3
calculate2:tdr:emphasis:cursor:post1 3

Query Syntax

CALCulate<cnum>:TDR:EMPHasis:CURSor:POST1?

Return Type

Double

Default

0


CALCulate<cnum>:TDR:EMPHasis:CURSor:POST2 <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the emphasis post2 level.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Post2 level value. The range is -20 dB to +20 dB.

Examples

CALC:TDR:EMPH:CURS:POST2 3
calculate2:tdr:emphasis:cursor:post2 3

Query Syntax

CALCulate<cnum>:TDR:EMPHasis:CURSor:POST2?

Return Type

Double

Default

0


CALCulate<cnum>:TDR:EMPHasis:CURSor:PRE1 <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the emphasis pre1 level.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Pre1 level value. The range is -20 dB to +20 dB.

Examples

CALC:TDR:EMPH:CURS:PRE1 2
calculate2:tdr:emphasis:cursor:pre1 2

Query Syntax

CALCulate<cnum>:TDR:EMPHasis:CURSor:PRE1?

Return Type

Double

Default

0


CALCulate<cnum>:TDR:EMPHasis:STATe <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) Turns the emphasis function state ON or OFF.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns emphasis ON.
OFF or 0
- Turns emphasis OFF.

Examples

CALC:TDR:EMPH:STAT ON
calculate2:tdr:emphasis:state off

Query Syntax

CALCulate<cnum>:TDR:EMPHasis:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:EQUalization:CTLE:DC <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the equalization CTLE (Continuous Time Linear Equalization) DC gain parameter.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

CTLE value. The range is 0 to 10.

Examples

CALC:TDR:EQU:CTLE:DC 0.077
calculate2:tdr:equalization:ctle:dc 0.077

Query Syntax

CALCulate<cnum>:TDR:EQUalization:CTLE:DC?

Return Type

Double

Default

0.667


CALCulate<cnum>:TDR:EQUalization:CTLE:POLE1 <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the equalization CTLE (Continuous Time Linear Equalization) Pole1 parameter.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

CTLE value. The range is 0 to 76E9 in Hz.

Examples

CALC:TDR:EQU:CTLE:POLE1 2E9
calculate2:tdr:equalization:ctle:pole1 2e9

Query Syntax

CALCulate<cnum>:TDR:EQUalization:CTLE:POLE1?

Return Type

Double

Default

1.95E9


CALCulate<cnum>:TDR:EQUalization:CTLE:POLE2 <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the equalization CTLE (Continuous Time Linear Equalization) Pole2 parameter.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

CTLE value. The range is 0 to 76E9 in Hz.

Examples

CALC:TDR:EQU:CTLE:POLE2 2E9
calculate2:tdr:equalization:ctle:pole2 2e9

Query Syntax

CALCulate<cnum>:TDR:EQUalization:CTLE:POLE2?

Return Type

Double

Default

5E9


CALCulate<cnum>:TDR:EQUalization:CTLE:ZERO1 <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the equalization CTLE (Continuous Time Linear Equalization) zero parameter.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

CTLE value. The range is 0 to 76E9 in Hz.

Examples

CALC:TDR:EQU:CTLE:ZERO1 650E6
calculate2:tdr:equalization:ctle:zero1 650e6

Query Syntax

CALCulate<cnum>:TDR:EQUalization:CTLE:ZERO1?

Return Type

Double

Default

650E6


CALCulate<cnum>:TDR:EQUalization:FILename <file>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the filename of the equalization equation user file. It is necessary to select the file using CALCulate:TDR:EQUalization:TYPE and turn ON the :CALCulate:TDR:EQUalization:STATe. This file is saved with .csv extension.

Specify the file name with the extension. When you use directory names (folder names) and file name, separate them with "\ " (back slash), or "/" (slash).

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<file>

Filename up to 254 characters.

Examples

CALC:TDR:EQU:FIL "C:\folder\User.csv"
calculate2:tdr:equalization:filename "C:\folder\User.csv"

Query Syntax

CALCulate<cnum>:TDR:EQUalization:FILename?

Return Type

String

Default

" " (Empty String)


CALCulate<cnum>:TDR:EQUalization:STATe <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) Turns the equalization function state ON or OFF.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns equalization ON.
OFF or 0
- Turns equalization OFF.

Examples

CALC:TDR:EQU:STAT ON
calculate2:tdr:equalization:state off

Query Syntax

CALCulate<cnum>:TDR:EQUalization:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:EQUalization:TYPE <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the equalization type.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Equalization type. Choose from:

EQUation - Option to enter values for equation calculation.

USER - Load user file.

Examples

CALC:TDR:EQU:TYPE EQU
calculate2:tdr:equalization:type equation

Query Syntax

CALCulate<cnum>:TDR:EQUalization:TYPE?

Return Type

Double

Default

EQUation


CALCulate<cnum>:TDR:EYE:EXECute 

Applicable Models: All with TDR Options (S9x011A/B)

(Write-only) This command performs the calculation for the simulated eye diagram for the active trace.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

Example

CALC:TDR:EYE:STAT ON
CALC:PAR:MNUM:SEL 3
CALC:TDR:EYE:EXEC


CALCulate<cnum>:TDR:EYE:INPut:BPATtern:LENGth <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the bits' power of 2 for a PRBS pattern. This value is used only when the selected bit pattern type is PRBS.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Bit pattern power of 2. The range is 3 to 15 (resolution is 1).

Examples

CALC:TDR:EYE:INP:BPAT:TYPE PRBS
CALC:TDR:EYE:INP:BPAT:LENG 7

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:BPATtern:LENGth?

Return Type

Integer

Default

7


CALCulate<cnum>:TDR:EYE:INPut:BPATtern:TYPE <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the bit pattern type for the simulated eye function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Eye pattern type. Choose from:

PRBS - Pseudo-Random Bit Sequence.

K285 - K 28.5.

USER - Custom user-defined pattern.

STAT - Statistical calculation.

Examples

CALC:TDR:EYE:INP:BPAT:TYPE K285
calculate2:tdr:eye:input:bpattern:type k285

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:BPATtern:TYPE?

Return Type

String

Default

PRBS


CALCulate<cnum>:TDR:EYE:INPut:DRATe <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the bit rate in bits/sec for the simulated eye function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Bit rate in bits/sec. The range is 1.21M to 60.8G.

Examples

CALC:TDR:EYE:INP:DRAT 1.1E9
calculate2:tdr:eye:input:drate 1.1e9

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:DRATe?

Return Type

Double

Default

1G


CALCulate<cnum>:TDR:EYE:INPut:JITTer:DLIMit <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the display limit value.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Display limit value. The range is 0 to 1.

Examples

CALC:TDR:EYE:INP:JITT:DLIM 0
calculate2:tdr:eye:input:jitter:dlimit 0

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:JITTer:DLIMit?

Return Type

Double

Default

1-E-9


CALCulate<cnum>:TDR:EYE:INPut:JITTer:PERiodic:FREQuency <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the periodic jitter frequency. This value is used only when the periodic jitter function type is selected.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Periodic jitter frequency in Hz. The range is 0 to TDR eye jitter max frequency.

Examples

CALC:TDR:EYE:INP:JITT:PER:FREQ 0
calculate2:tdr:eye:input:jitter:periodic:frequency 0

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:JITTer:PERiodic:FREQuency?

Return Type

Double

Default

500E3


CALCulate<cnum>:TDR:EYE:INPut:JITTer:PERiodic:MAGNitude <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the periodic jitter magnitude in rms. This value is used only when periodic jitter function type is selected.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Periodic jitter magnitude. The range is 0 to 1 UI.

Examples

CALC:TDR:EYE:INP:JITT:TYPE:PER
CALC:TDR:EYE:INP:JITT:PER:MAGN 0.5

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:JITTer:PERiodic:MAGNitude?

Return Type

Double

Default

0


CALCulate<cnum>:TDR:EYE:INPut:JITTer:RANDom:MAGNitude <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the random jitter magnitude in rms. This value is used only when random jitter function type is selected.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Random jitter magnitude. The range is 0 to 0.25 UI.

Examples

CALC:TDR:EYE:INP:JITT:TYPE:RAND
CALC:TDR:EYE:INP:JITT:RAND:MAGN 0.05

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:JITTer:RANDom:MAGNitude?

Return Type

Double

Default

0


CALCulate<cnum>:TDR:EYE:INPut:JITTer:STATe <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) Turns the jitter function state with simulated eye ON or OFF.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns jitter ON.
OFF or 0
- Turns jitter OFF.

Examples

CALC:TDR:EYE:INP:JITT:STAT ON
calculate2:tdr:eye:input:jitter:state off

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:JITTer:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:EYE:INPut:JITTer:TYPE <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the jitter function type for the simulated eye function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Jitter type. Choose from:

RANDom - Random jitter function.

PERiodic - Periodic jitter function.

Examples

CALC:TDR:EYE:INP:JITT:TYPE RAND
calculate2:tdr:eye:input:jitter:type random

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:JITTer:TYPE?

Return Type

String

Default

PERiodic


CALCulate<cnum>:TDR:EYE:INPut:OLEVel <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the voltage level for bit "1" for the simulated eye function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Level for bit "1". The range is -5 V to +5 V.

Examples

CALC:TDR:EYE:INP:OLEV 100E-3
calculate2:tdr:eye:input:olevel 100e-3

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:OLEVel?

Return Type

Double

Default

0.2


CALCulate<cnum>:TDR:EYE:INPut:RTIMe:DATA <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the rise time value for the simulated eye function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Rise time for simulated eye function in seconds.

Examples

CALC:TDR:EYE:INP:RTIM:DATA 90E-12
calculate2:tdr:eye:input:rtime:data 90e-12

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:RTIMe:DATA?

Return Type

Double

Default

35E-12


CALCulate<cnum>:TDR:EYE:INPut:RTIMe:THReshold <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the rise time threshold for the simulated eye.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Threshold levels. Choose from:

T1_9 - 10% to 90%.

T2_8 - 20% to 80%.

Examples

CALC:TDR:EYE:INP:RTIM:THR T1_9
calculate2:tdr:eye:input:rtime:threshold t1_9

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:RTIMe:THReshold?

Return Type

String

Default

T1_9


CALCulate<cnum>:TDR:EYE:INPut:ZLEVel <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the voltage level for bit "0" for the simulated eye function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Voltage level for bit "0". The range is -5 V to +5 V.

Examples

CALC:TDR:EYE:INP:ZLEV 100E-3
calculate2:tdr:eye:input:zlevel 100e-3

Query Syntax

CALCulate<cnum>:TDR:EYE:INPut:ZLEVel?

Return Type

Double

Default

0


CALCulate<cnum>:TDR:EYE:MASK:FAIL?

Applicable Models: All with TDR Options (S9x011A/B)

(Read-only) This command returns the mask test result.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

Examples

CALC:TDR:EYE:MASK:FAIL?
calculate2:tdr:eye:mask:fail?

Return Type

Boolean

ON or 1 - Mask test fail.
OFF or 0
- Mask test pass.

Default

Not Applicable


CALCulate<cnum>:TDR:EYE:MASK:STATe <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) Turns the mask test function state with simulated eye ON or OFF.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns mask test ON.
OFF or 0
- Turns mask test OFF.

Examples

CALC:TDR:EYE:MASK:STAT ON
calculate2:tdr:eye:mask:state off

Query Syntax

CALCulate<cnum>:TDR:EYE:MASK:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:EYE:RESults:DATA?

Applicable Models: All with TDR Options (S9x011A/B)

(Read-only) This command returns the results of the eye measurement. There are 18 values returned. The minimum and maximum values are returned in addition to the displayed results (16 values) on the TDR application GUI.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

Examples

CALC:TDR:EYE:RESults:DATA?
calculate2:tdr:eye:results:data?

Return Type

Variant Array

Default

Not Applicable


CALCulate<cnum>:TDR:EYE:RESults:DISPlay:STATe <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) Turns the overlay ON or OFF.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns overlay ON.
OFF or 0
- Turns overlay OFF.

Examples

CALC:TDR:EYE:RES:DISP:STAT ON
calculate2:tdr:eye:results:display:state off

Query Syntax

CALCulate<cnum>:TDR:EYE:RESulsts:DISPlay:STATe?

Return Type

Boolean

Default

ON


CALCulate<cnum>:TDR:EYE:RESults:THReshold <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the rise time threshold level for the results of eye measurement.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Threshold levels. Choose from:

T1_9 - 10% to 90%.

T2_8 - 20% to 80%.

Examples

CALC:TDR:EYE:RES:THR T1_9
calculate2:tdr:eye:results:threshold t1_9

Query Syntax

CALCulate<cnum>:TDR:EYE:RESults:THReshold?

Return Type

String

Default

T1_9


CALCulate<cnum>:TDR:EYE:STATe <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) Turns the Eye/Mask window ON or OFF.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns Eye/Mask window ON.
OFF or 0
- Turns Eye/Mask window OFF.

Examples

CALC:TDR:EYE:STAT ON
calculate2:tdr:eye:state off

Query Syntax

CALCulate<cnum>:TDR:EYE:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:MEASure[1-256]:ACTive:MARKer <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets active marker number.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Marker number to activate. The range is 0 to 10.

Examples

CALC:TDR:MEAS1:ACT:MARK 1
calculate2:tdr:measure1:active:marker 1

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:ACTive:MARKer?

Return Type

Integer

Default

0


CALCulate<cnum>:TDR:MEASure[1-256]:DTIMe:DATA?

Applicable Models: All with TDR Options (S9x011A/B)

(Read-only) This command returns the delta time result value. You can get the result even if CALCulate:TDR:MEASure:DTIMe:STATe is off.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

Examples

CALC:TDR:MEAS1:DTIM:DATA?
calculate2:tdr:measure1:dtime:data?

Return Type

Double

Default

Not Applicable


CALCulate<cnum>:TDR:MEASure[1-256]:DTIMe:POSition <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets delta time reference position.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Delta time reference position. The range is 0 to 100.

Examples

CALC:TDR:MEAS1:DTIM:POS 0
calculate2:tdr:measure1:dtime:position 0

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:DTIMe:POSition?

Return Type

Double

Default

50


CALCulate<cnum>:TDR:MEASure[1-256]:DTIMe:STATe <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) Turns the delta time marker in the marker search ON or OFF.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns delta time marker ON.
OFF or 0
- Turns delta time marker OFF.

Examples

CALC:TDR:MEAS1:DTIM:STAT ON
calculate2:tdr:measure1:dtime:state off

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:DTIMe:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:MEASure[1-256]:DTIMe:TARGet <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the target trace number for the delta time function. The MEASure[1-256] is the trace number starting point for delta time. The <value> is the trace number stopping point for delta time.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Trace number stopping point for delta time. The range is 1 to 16.

Examples

CALC:TDR:MEAS1:DTIM:TARG 5
calculate2:tdr:measure1:dtime:target 5

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:DTIMe:TARGet?

Return Type

Integer

Default

1


CALCulate<cnum>:TDR:MEASure[1-256]:FORMat <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the trace format.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Trace format.

For S-Parameter measurements, choose from:

MLINear

MLOGarithmic

PHASe

UPHase

IMAGinary

REAL

POLar

SMITh

SADMittance

SWR

GDELay

KELVin|

FAHRenheit

CELSius

PPHase

IMPedance

VOLT

 

For Time Domain measurements, choose from:

IMPedance

VOLT

MLOGarithmic

MLINear

REAL

Examples

CALC:TDR:MEAS1:FORM IMP
calculate2:tdr:measure1:format impedance

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:FORMat?

Return Type

String

Default

MLINear


CALCulate<cnum>:TDR:MEASure[1-256]:MARKer:REFerence[:STATe] <ON | OFF>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) Turns the reference marker ON or OFF.

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<ON | OFF>

ON (or 1) - turns reference marker ON

OFF (or 0) - turns reference marker ON

Examples

CALC:TDR:MEAS1:MARK:REF ON
calculate2:tdr:measure1:marker:reference:state OFF

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:MARKer:REFerence[:STATe]?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:MEASure[1-256]:MARKer<mkr>[:STATe] <ON|OFF>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) Turns the specified marker ON or OFF.

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1.

<mkr>

Any marker number from 1 to 15; if unspecified, value is set to 1.

<ON|OFF>

ON (or 1) - turns marker ON.

OFF (or 0) - turns marker OFF.

Examples

CALC:TDR:MEAS:MARK ON
calculate2:tdr:measure2:marker8 on

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:MARKer<mkr>:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:MEASure[1-256]:PARameter <string> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the measurement parameter.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<sting>

Measurement parameter.

For S-Parameter measurements::

Sxy

Sddxy

Sdcxy

Scdxy

Sccxy

X: 1 to 4

Y: 1 to 4

 

For Time Domain measurements:

Txy

Tddxy

Tdcxy

Tcdxy

Tccxy

Examples

CALC:TDR:MEAS1:PAR T11
calculate2:tdr:measure1:parameter t11

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:PARameter?

Return Type

String

Default

S11


CALCulate<cnum>:TDR:MEASure[1-256]:PEELing:STATe <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets state for the peeling function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns peeling function ON.
OFF or 0
- Turns peeling function OFF.

Examples

CALC:TDR:MEAS1:PEEL:STAT ON
calculate2:tdr:measure1:peeling:state off

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:PEELing:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:MEASure[1-256]:SMOothing:STATe <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets state for the smoothing function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns smoothing function ON.
OFF or 0
- Turns smoothing function OFF.

Examples

CALC:TDR:MEAS1:SMO:STAT ON
calculate2:tdr:measure1:smoothing:state off

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:SMOothing:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:MEASure[1-256]:TIME:IMPulse:WIDTh <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the impulse width value for the transform function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Transform function impulse width value.

Examples

CALC:TDR:MEAS1:TIME:IMP:WIDT 17E-12
calculate2:tdr:measure1:time:impulse:width 17e-12

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:TIME:IMPulse:WIDTh?

Return Type

Double

Default

0


CALCulate<cnum>:TDR:MEASure[1-256]:TIME:STEP:COUPle <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command enables/disables rise time coupling.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns  rise time coupling ON.
OFF or 0
- Turns rise time coupling OFF.

Examples

CALC:TDR:MEAS:TIME:STEP:COUP ON
calculate2:tdr:meas:time:step:couple off

Query Syntax

CALCulate<cnum>:TDR:MEAS:TIME:STEP:COUPle?

Return Type

Boolean

Default

ON


CALCulate<cnum>:TDR:MEASure[1-256]:TIME:STEP:RTIMe <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets rise time value for the transform function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Transform function rise time value in seconds.

Examples

CALC:TDR:MEAS1:TIME:STEP:RTIM 0
calculate2:tdr:measure1:time:step:rtime 0

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:TIME:STEP:RTIMe?

Return Type

Double

Default

0


CALCulate<cnum>:TDR:MEASure[1-256]:TIME:STEP:RTIMe:THReshold <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the rise time threshold level for the results of eye measurement.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Transform function rise time threshold levels. Choose from:

T1_9 - 10% to 90%.

T2_8 - 20% to 80%.

Examples

CALC:TDR:MEAS1:TIME:STEP:RTIM:THR T1_9
calculate2:tdr:measure1:time:step:rtime:threshold t1_9

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:TIME:STEP:RTIMe:THReshold?

Return Type

String

Default

T1_9


CALCulate<cnum>:TDR:MEASure[1-256]:TIME:TYPE <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the stimulus type for the transform function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Transform function stimulus type. Choose from:

LPSTep - Low pass step.

LPIMpulse -Low pass impulse.

Examples

CALC:TDR:MEAS1:TIME:TYPE LPST
calculate2:tdr:measure1:time:type lpstep

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:TIME:TYPE?

Return Type

String

Default

LPSTep


CALCulate<cnum>:TDR:MEASure[1-256]:TTIMe:DATA?

Applicable Models: All with TDR Options (S9x011A/B)

(Read-only) This command returns the rise time result value for marker search. You can get the data even if  CALCulate:TDR:MEASure:TTIMe:STATe is off.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

Examples

CALC:TDR:MEAS1:TTIM:DATA?
calculate2:tdr:measure1:ttime:data?

Return Type

Double

Default

Not Applicable


CALCulate<cnum>:TDR:MEASure[1-256]:TTIMe:STATe <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command displays the rise time marker.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns rise time marker ON.
OFF or 0
- Turns rise time marker OFF.

Examples

CALC:TDR:MEAS1:TTIM:STAT ON
calculate2:tdr:measure1:ttime:state off

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:TTIMe:STATe?

Return Type

Boolean

Default

OFF


CALCulate<cnum>:TDR:MEASure[1-256]:TTIMe:THReshold <enum> 

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the rise time threshold for the rise time in the marker search function.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<enum>

Rise time threshold levels. Choose from:

T1_9 - 10% to 90%.

T2_8 - 20% to 80%.

Examples

CALC:TDR:MEAS1:TTIM:THR T1_9
calculate2:tdr:measure1:ttime:threshold t1_9

Query Syntax

CALCulate<cnum>:TDR:MEASure[1-256]:TTIMe:THReshold?

Return Type

String

Default

T1_9


CALCulate<cnum>:TDR:TIME:COUPle <bool>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command enables/disables time coupling.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<bool>

ON or 1 - Turns  time coupling ON.
OFF or 0
- Turns time coupling OFF.

Examples

CALC:TDR:TIME:COUP ON
calculate2:tdr:time:couple off

Query Syntax

CALCulate<cnum>:TDR:TIME:COUPle?

Return Type

Boolean

Default

ON


CALCulate<cnum>:TDR:TIME:STEP:AMPLitude <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets or gets the step amplitude value.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Step amplitude value in Hz, dBm, or seconds. The range is 0.001 to 5.

Examples

CALC:TDR:TIME:STEP:AMPL 200ms
calculate2:tdr:time:step:amplitude .05s

Query Syntax

CALCulate<cnum>:TDR:TIME:STEP:AMPLitude?

Return Type

Double

Default

0.2