Route Command


Learn about Frequency Offset

SCPI Command Tree

 

ROUTe<cnum>:PATH:LOOP[:R1] <char>

Applicable Models: N522xB, N524xB

(Read-Write)  Throws internal switch to reference receiver when the specified channel is measured.

N523xA models do NOT have the R1 reference receiver switch.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<char>

Position of the switch. Choose from:

INTernal - bypass R1 Loop.  Connects the port 1 source directly to the R1 receiver.

EXTernal - flow through R1 Loop.  Allows direct access to the R1 receiver through the Reference 1 front-panel connectors.

Examples

ROUT:PATH:LOOP INT
route2:path:loop:r1 external

Query Syntax

ROUTe<cnum>:PATH:LOOP:R1?

Return Type

Character

Default

INTernal