Sense:Couple Commands


Click on a keyword to view the command details.

See Also


SENSe<cnum>:COUPle <ALL | NONE> OBSOLETE

This command is not necessary, and its use is not recommended. Setting the sweep mode to NONE does not improve the quality of the measurement.

Applicable Models: All

(Read-Write) Sets the sweep mode as Chopped or Alternate.

Learn about Alternate Sweep

Parameters

 

<cnum>

Any existing channel number; if unspecified, value is set to 1.

<ALL | NONE>

ALL - Sweep mode set to Chopped - reflection and transmission measured on the same sweep.

NONE - Sweep mode set to Alternate - reflection and transmission measured on separate sweeps. Increases sweep time

Examples

SENS:COUP ALL
sense2:couple none

Query Syntax

SENSe<cnum>:COUPle?

Return Type

Character

Default

ALL


SENSe<cnum>:COUPle:PARameter[:STATe] <bool>

Applicable Models: All

(Read-Write)  Turns ON and OFF Time Domain Trace Coupling. All of the measurements in the specified channel are coupled.

Learn more about Time Domain Trace Coupling.

Parameters

 

<cnum>

Any existing channel number; if unspecified, value is set to 1.

<bool>

ON (or 1) - Turns ON Time Domain Trace Coupling.

OFF (or 0) - Turns OFF Time Domain Trace Coupling.

Examples

SENS:COUP:PAR 0
sense2:couple:parameter:state on

Query Syntax

SENSe<cnum>:COUPle:PARameter[:STATe]?

Return Type

Boolean

Default

ON (or 1)