Controls and queries settings related with Service.
| SERVice: | 
Applicable Models: ALL
| (Read-Write) Set/get trace sNp file for dummy DUT. Preset & Save/Recall does not work for this command. This command is replaced by SYST:SIM:DUT:FILE | |
| Parameters | <string> sNp file to be set to dummy DUT | 
| Examples | SERV:DUMM:DUT:FILE? | 
| Return Type | string | 
| Not Applicable | |
Applicable Models: ALL
| (Read-Write) Set/get trace noise state for dummy DUT Preset & Save/Recall does not work for this command This command is replaced by SYST:SIM:DUT:NOIS | |
| Parameters | <bool> Noise state. | 
| Examples | SERV:DUMM:DUT:NOIS:STAT? | 
| Return Type | bool | 
| ON | |
Applicable Models: E5080A/B, M9485A, M98xxA, P50xxA/B
| (Write-only) Delete the service error log files stored in the modules and PC. See Error Log. | |
| Parameters | 
 | 
| Examples | SERV:LOGG:CLE | 
| Return Type | N/A | 
| Not Applicable | |