SYSTem:CHANnels:GCSetup commands

Configures and makes settings for GCA Parallel measurements.

SYSTem:CHANnels:GCSetup:

| PARallel

| [:ENABle]

| GROup

Click on a red keyword to view the command details.

See Also


SYSTem:CHANnels:GCSetup:PARallel[:ENABle] <bool>

Applicable Models: M980xA, M983xA

(Read-Write) Sets and reads the GCA Parallel Measurement state.

Parameters

<bool>

Choose from:

ON or 1: GCA parallel measurement are enabled.

OFF or 0: GCA parallel measurement are disabled..

Examples

SYST:CHAN:GCS:PAR:ENAB ON

system:channels:gcsetup:parallel:enable 0

Query Syntax

SYSTem:CHANnels:GCSetup:PARallel:ENABle?

Default

OFF


SYSTem:CHANnels:GCSetup:PARallel:GROup <iarray>

Applicable Models: M980xA, M983xA

(Read-Write) Sets and reads the group of channels for the GCA Parallel Measurement.

Parameters

<iarray>

{<number of group>, <start channel No. of group #1>, <end channel No. of group #1>, <start channel No. of group #2>, <end channel No. of group #2>, ... }

The first item means number or groups.

Next pairs show start/end channel numbers of the group. 1 pair for 1 group.

Example:

{0} - Couples all existing GCA channels in one group (default setting)

{1,1,4} - Couples channel 1-4 in one group

{2,1,3,5,7} - Couples channel 1-3 in first group and channels 5-7 in second group

Examples

SYST:CHAN:GCS:PAR:GRO 2,1,3,5,7

system:channels:gcsetup:parallel:group 1,1,4

Query Syntax

SYSTem:CHANnels:GCSetup:PARallel:GROup?

Default

0