SOURce:TDR Commands

SOURce:TDR

POWer

       | LEVel

          | IMMediate

               | AMPLitude

 

Click on a red keyword to view the command details.

See Also


SOURce<cnum>:TDR:POWer[:LEVel][:IMMediate][:AMPLitude] <value>

Applicable Models: All with TDR Options (S9x011A/B)

(Read-Write) This command sets the source power level.

Parameters

 

<cnum>

Channel number of the measurement. If unspecified, <cnum> is set to 1.

<value>

Source power level in dBm.

Examples

SOUR:TDR:POW 20

source:tdr:power:level:immediate:amplitude 20

Query Syntax

SOURce:TDR:POWer[:LEVel][:IMMediate][:AMPLitude]?

Return Type

Double

Default

-8 dBm