AFR Using One Single-Ended OPEN


This VBScript program performs AFR using one single-ended OPEN, saves the fixture data to a file, then performs deembedding.

Each VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the code into a text editor file, such as Notepad, and save it on the PNA hard drive as *.vbs.

See Also:

Learn how to setup and run the macro

SCPI Example Programs

Dim app
Dim scpi
Set app = CreateObject("AgilentPNA835x.Application")
Set scpi = app.ScpiStringParser

'The AOPen data file should alreay exist
aopenFile = "S:\case_05\AOpen.s1p"
'Fixture data file will be created or overwritten
fixaFile = "S:\case_05\_demo_fix_a.s2p"

'AFR extracts fixture files
scpi.Execute("AFR:INITialize")
scpi.Execute("AFR:FIXTure:MEASurement 1")
scpi.Execute("AFR:STANdard:USE AOPen")
scpi.Execute("AFR:STANdard:LOAD AOPen," & Q(aopenFile))
scpi.Execute("AFR:SAVE:PORTs VNA")
scpi.Execute("AFR:SAVE:FILename " & Q(fixaFile))
opc = scpi.Execute("*OPC?")

' deembedding
scpi.Execute("CALC:FSIM:SEND:DEEM:PORT1:USER:FILename " & Q(fixaFile))
scpi.Execute("CALC:FSIM:SEND:DEEM:PORT1:TYPE USER")
scpi.Execute("CALC:FSIM:SEND:DEEM:STATe ON")
scpi.Execute("CALC:FSIM:STATe ON")
opc = scpi.Execute("*OPC?")

Set scpi = Nothing
Set app = Nothing

'Add double quotation marks to a string
Function Q(s)
 Q = Chr(34) & s & Chr(34)
End Function