|
'------------------------------------------ ' create NF channel '------------------------------------------ SYST:FPRESET DISP:WIND:STATE ON CALC1:MEAS1:DEF "S11:Noise Figure Cold Source" DISP:MEAS1:FEED 1 CALC1:MEAS2:DEF "NF:Noise Figure Cold Source" DISP:MEAS2:FEED 1 '------------------------------------------ ' configure power sensor '------------------------------------------ system:communicate:psensor usb, "Agilent Technologies,U8485A,MY53470003" '------------------------------------------ ' configure calibrate all '------------------------------------------ SYST:CAL:ALL:RESET SYST:CAL:ALL:CSET:PREFIX "Example" SYST:CAL:ALL:SEL 1 SYST:CAL:ALL:CHAN1:PORTS:SEL 1,2 '------------------------------------------ ' use this query to see what cal all properties are ' relevant to the noise figure channel '------------------------------------------ SYST:CAL:ALL:MCLASS:PROP:NAME:CAT? "Noise Figure Cold Source" '------------------------------------------ ' set scalar noise cal, using power meter '------------------------------------------ SYST:CAL:ALL:MCLASS:PROP:VAL:STATE "Noise Cal Method", "Scalar" SYST:CAL:ALL:MCLASS:PROP:VAL:STATE "Receiver Characterization Method", "Use Power Meter" '------------------------------------------ ' retrieve the guided cal channel number '------------------------------------------ SYST:CAL:ALL:GUIDED:CHAN? ' configure the sensor ' set ignored unless you want to calibrate ' an adapter used for the power sensor. SENS200:CORR:COLL:GUID:PSEN1:CONN 'Ignored' SENS200:CORR:COLL:GUID:PSEN1:CKIT 'Not used' SENS200:CORR:COLL:GUID:PSEN1:POW:LEV -15 '------------------------------------------------- ' configure basic cal properties: connectors, kits ' NOTE: always fully specify ecals when Noise figure ' is in the channel list. IE: include the ecal serial ' number! '------------------------------------------------- SENS200:CORR:COLL:GUID:CONN:PORT1:SEL "APC 3.5 male" SENS200:CORR:COLL:GUID:CONN:PORT2:SEL "APC 3.5 female" SENS200:CORR:COLL:GUID:ckit:port2:SEL "N4691-60004 ECal 02297" SENS200:CORR:COLL:GUID:ckit:port1:SEL "N4691-60004 ECal 02297" SENS200:CORR:COLL:GUID:INIT ' acquire the calibration SENS200:CORR:COLL:GUID:STEPS? SENS200:CORR:COll:guid:DESC? 1 SENS200:CORR:COLL:GUID:ACQ STAN1 SENS200:CORR:COLL:GUID:desc? 2 SENS200:CORR:COLL:GUID:ACQ STAN2 SENS200:CORR:COLL:GUID:desc? 3 SENS200:CORR:COLL:GUID:ACQ STAN3 SENS200:CORR:COLL:GUID:SAVE |
The channel number used for the SENSe header is determined by the SYST:CAL:ALL:GUID:CHAN? command. You must query this channel number – do not assume that it will always be a particular value.