'------------------------------------------ ' create a standard channel '------------------------------------------ DISPlay:WINDow1:STATE ON CALC1:PARameter:DEFine:EXT "MyMeas", S21 DISPlay:WINDow1:TRACe1:FEED "MyMeas" SENSe1:BANDwidth 700 SENSe1:FREQuency:CENTer 1ghz SENSe1:FREQuency:SPAN 1ghz SENSe1:SWEep:POINts 11 '------------------------------------------ ' create a Mixer channel '------------------------------------------ DISPlay:WINDow2:STATE ON CALC2:CUST:DEF 'My SC21', 'Scalar Mixer/Converter', 'SC21' DISP:WIND2:TRAC:FEED 'My SC21' SENS2:SWEep:POINts 11 SENS2:BANDwidth 1e3 SENS2:MIX:INPut:FREQ:MODE SWEPt SENS2:MIX:INPut:FREQ:STAR 3.6e9 SENS2:MIX:INPut:FREQ:STOP 3.9e9 SENS2:MIX:LO:FREQ:MODE FIXED SENS2:MIX:LO:FREQ:FIX 1.0e9 SENS2:MIX:LO:POW 10 SENS2:MIX:OUTP:FREQ:SID LOW SENS2:MIX:CALC Output SENS2:MIX:LO:NAME 'Port 3' SENS2:MIX:APPLY '------------------------------------------ ' configure cal all '------------------------------------------ SYST:CAL:ALL:RESet SYST:CAL:ALL:SEL 1,2 SYST:CAL:ALL:IFBW 1e3 SYST:CAL:ALL:PORT1:SOUR:POWer -10 SYST:CAL:ALL:CSET:PREFix 'MyCalAllExample' '----------------------------------------------------- ' query for the available mixer cal properties to set ' this is an info only query '----------------------------------------------------- SYST:CAL:ALL:MCL:PROP:NAME:CAT? 'Scalar Mixer/Converter' SYST:CAL:ALL:MCL:PROP:VAL:CAT? 'Phase Correction Method' SYST:CAL:ALL:MCL:PROP:VAL:CAT? 'Mixer Delay' '------------------------------------------------------------- ' Enable phase correction using a cal mixer with known delay '------------------------------------------------------------- SYST:CAL:ALL:MCL:PROP:VAL 'Enable Phase Correction','true' SYST:CAL:ALL:MCL:PROP:VAL 'Phase Correction Method','Use Mixer Delay' SYST:CAL:ALL:MCL:PROP:VAL 'Mixer Delay', '10e-9' '------------------------------------------------------------- ' configure power sensor '------------------------------------------------------------- SYST:COMM:PSEN USB, "Agilent Technologies,U8485A,my53470003" '------------------------------------------------------------- ' Perform calibration '------------------------------------------------------------- SYST:CAL:ALL:GUIDed:CHAN? SENS200:corr:coll:guid:conn:port1 "APC 3.5 male" SENS200:corr:coll:guid:conn:port2 "APC 3.5 female" SENS200:corr:coll:guid:conn:port3 "Not used" SENS200:corr:coll:guid:conn:port4 "Not used" SENS200:corr:coll:guid:ckit:port1 "N4691-60004 ECal" SENS200:corr:coll:guid:ckit:port2 "N4691-60004 ECal" SENS200:corr:coll:guid:init SENS200:corr:coll:guid:steps? SENS200:corr:coll:guid:acq stan1 SENS200:corr:coll:guid:acq stan2 SENS200:CORR:COLL:GUID:desc? 3 SENS200:corr:coll:guid:acq stan3 SENS200:CORR:COLL:GUID:SAVE |
The channel number used for the SENSe header is determined by the SYST:CAL:ALL:GUID:CHAN? command. You must query this channel number – do not assume that it will always be a particular value.