|
Set pna = CreateObject("AgilentPNA835x.Application") Set scpi = pna.ScpiStringParser scpi.Parse "SYST:PRESET" scpi.Parse "calc:par:del:all" scpi.Parse "calc:cust:def 'sc12','Scalar Mixer/Converter','SC12'" scpi.Parse "disp:wind:trac1:feed 'sc12'" scpi.Parse "*OPC?" scpi.Parse "SYST:CAL:ALL:RESet" scpi.Parse "syst:cal:all:sel 1" scpi.Parse "SYST:CAL:ALL:CSET:PREFix 'smcSplit'" scpi.Parse "syst:cal:all:chan1:port:sel 1,2" scpi.Parse "syst:cal:all:mcl:prop:val 'Include Power Calibration','true'" 'Split Cal attribute MUST be sent before setting connectors & kits scpi.Parse "SYST:CAL:ALL:MCL:PROP:VAL 'Split Cal', 'True'" scpi.Parse "SYST:CAL:ALL:GUID:CHAN?" scpi.Parse "SENS200:CORR:COLL:GUID:CONN:PORT1 'APC 3.5 male'" scpi.Parse "SENS200:CORR:COLL:GUID:CONN:PORT2 'APC 3.5 male'" scpi.Parse "SENS200:CORR:COLL:GUID:CKIT:PORT1 '85052D'" scpi.Parse "SENS200:CORR:COLL:GUID:CKIT:PORT2 '85052D'" scpi.Parse "SENS200:CORR:COLL:GUID:INIT" scpi.Parse "SENS200:CORR:COLL:GUID:STEP?" 'Note that Step 1 is to connect Power Sensor to Port 1 'And Step 2 is to connect Power Sensor to Port 2 'Performing two 1-Port calibrations instead of a 2-port calibration scpi.Parse "SENS200:CORR:COLL:GUID:DESC? 1" scpi.Parse "SENS200:CORR:COLL:GUID:DESC? 2" scpi.Parse "SENS200:CORR:COLL:GUID:DESC? 3" scpi.Parse "SENS200:CORR:COLL:GUID:DESC? 4" scpi.Parse "SENS200:CORR:COLL:GUID:DESC? 5" scpi.Parse "SENS200:CORR:COLL:GUID:DESC? 6" scpi.Parse "SENS200:CORR:COLL:GUID:DESC? 7" scpi.Parse "SENS200:CORR:COLL:GUID:DESC? 8" scpi.Parse "SENS200:CORR:COLL:GUID:ACQ STAN1;" scpi.Parse "SENS200:CORR:COLL:GUID:ACQ STAN2;" scpi.Parse "SENS200:CORR:COLL:GUID:ACQ STAN3;" scpi.Parse "SENS200:CORR:COLL:GUID:ACQ STAN4;" scpi.Parse "SENS200:CORR:COLL:GUID:ACQ STAN5;" scpi.Parse "SENS200:CORR:COLL:GUID:ACQ STAN6;" scpi.Parse "SENS200:CORR:COLL:GUID:ACQ STAN7;" scpi.Parse "SENS200:CORR:COLL:GUID:ACQ STAN8;" scpi.Parse "sens200:corr:coll:guid:save;*opc?" |
The channel number used for the SENSe header is determined by the SYST:CAL:ALL:GUID:CHAN? command. You must query this channel number – do not assume that it will always be a particular value.