Cal All for Mixer Channel

*CLS

 SYST:FPReset

'------------------------------------------

' create a standard channel

'------------------------------------------

 DISPlay:WINDow1:STATE ON

 CALC1:PARameter:DEFine:EXT "MyMeas", S21

 DISPlay:WINDow1:TRACe1:FEED "MyMeas"

 SENSe1:BANDwidth 700

 SENSe1:FREQuency:CENTer 1ghz

 SENSe1:FREQuency:SPAN 1ghz

 SENSe1:SWEep:POINts 11

'------------------------------------------

' create a Mixer channel

'------------------------------------------

 DISPlay:WINDow2:STATE ON

 CALC2:CUST:DEF 'My SC21', 'Scalar Mixer/Converter', 'SC21'

 DISP:WIND2:TRAC:FEED 'My SC21'

 SENS2:SWEep:POINts 11

 SENS2:BANDwidth 1e3

 SENS2:MIX:INPut:FREQ:MODE SWEPt

 SENS2:MIX:INPut:FREQ:STAR 3.6e9

 SENS2:MIX:INPut:FREQ:STOP 3.9e9

 SENS2:MIX:LO:FREQ:MODE FIXED

 SENS2:MIX:LO:FREQ:FIX 1.0e9

 SENS2:MIX:LO:POW 10

 SENS2:MIX:OUTP:FREQ:SID LOW

 SENS2:MIX:CALC Output

 SENS2:MIX:LO:NAME 'Port 3'

 SENS2:MIX:APPLY

'------------------------------------------

' configure cal all

' select channels 1 and 2.

' for channel 2 select all the ports of the mixer

' explicitly because we want to add the LO (port 3)

'------------------------------------------

 SYST:CAL:ALL:RESet

 SYST:CAL:ALL:SEL 1,2

 SYST:CAL:ALL:CHAN2:PORT:SEL 1,2,3

 SYST:ERR?

 SYST:CAL:ALL:CHAN2:PORT:SEL?

 SYST:CAL:ALL:IFBW 1e3

 SYST:CAL:ALL:PORT1:SOUR:POWer -10

 SYST:CAL:ALL:CSET:PREFix 'MyCalAllExample'

'-----------------------------------------------------

' query for the available mixer cal properties to set

' this is an info only query

'-----------------------------------------------------

 SYST:CAL:ALL:MCL:PROP:NAME:CAT? 'Scalar Mixer/Converter'

 SYST:CAL:ALL:MCL:PROP:VAL:CAT? 'Phase Correction Method'

 SYST:CAL:ALL:MCL:PROP:VAL:CAT? 'Mixer Delay'

  

'-------------------------------------------------------------

' Enable phase correction using a cal mixer with known delay

'-------------------------------------------------------------

 SYST:CAL:ALL:MCL:PROP:VAL 'Enable Phase Correction','true'

 SYST:CAL:ALL:MCL:PROP:VAL 'Phase Correction Method','Use Mixer Delay'

 SYST:CAL:ALL:MCL:PROP:VAL 'Mixer Delay', '10e-9'

'-------------------------------------------------------------

' configure power sensor

'-------------------------------------------------------------

 SYST:COMM:PSEN USB, "Agilent Technologies,U8485A,my53470003"

'-------------------------------------------------------------

' Perform calibration

' Note: the channel number used in the following SENS

'       commands MUST BE the channel number returned

'       from the preceding query SYST:CAL:ALL:GUIDed:CHAN?

'-------------------------------------------------------------

SYST:CAL:ALL:GUIDed:CHAN?

SENS200:corr:coll:guid:conn:port1 "APC 3.5 male"

SENS200:corr:coll:guid:conn:port2 "APC 3.5 female"

SENS200:corr:coll:guid:conn:port3 "Not used"

SENS200:corr:coll:guid:conn:port4 "Not used"

SENS200:corr:coll:guid:ckit:port1 "N4691-60004 ECal"

SENS200:corr:coll:guid:ckit:port2 "N4691-60004 ECal"

SENS200:corr:coll:guid:init; *OPC?

SENS200:corr:coll:guid:steps?

SENS200:CORR:COLL:GUID:desc? 1

SENS200:corr:coll:guid:acq stan1;*OPC?

SENS200:CORR:COLL:GUID:desc? 2

SENS200:corr:coll:guid:acq stan2;*OPC?

SENS200:CORR:COLL:GUID:desc? 3

SENS200:corr:coll:guid:acq stan3;*OPC?

SENS200:CORR:COLL:GUID:desc? 4

SENS200:corr:coll:guid:acq stan4;*OPC?

SENS200:CORR:COLL:GUID:SAVE;*OPC?

'--------------------------------------------------------------------------------

The channel number used for the SENSe header is determined by the SYST:CAL:ALL:GUID:CHAN? command. You must query this channel number – do not assume that it will always be a particular value.