The following SCPI example demonstrates how to create a Pulse Profile measurement using the Integrated Pulse Application on the PNA-X and N522xB.
Four measurements are created:
S11 (default)
S21
B receiver
R1 receiver - used to verify pulse gen settings.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as PulseProfile.vbs. Learn how to setup and run the macro.
Integrated Pulse Application
SCPI commands used in the program.
SCPI commands to control the internal pulse generators
|
' VNA application object Dim oPNA ' Channel 1 object Dim chan1 ' Create / Get the VNA application. Set oPNA = CreateObject("AgilentPNA835x.Application") dim scpi Set scpi = oPNA.ScpiStringParser scpi.parse "syst:preset" scpi.parse "CALCulate:PARameter:DEFine:EXT 'MyMeas1',S21" scpi.parse "DISPlay:WINDow1:TRACe2:FEED 'MyMeas1'" scpi.parse "CALCulate:PARameter:DEFine:EXT 'MyMeas2',R_1" scpi.parse "DISPlay:WINDow1:TRACe3:FEED 'MyMeas2'" scpi.parse "CALCulate:PARameter:DEFine:EXT 'MyMeas3',B_1" scpi.parse "DISPlay:WINDow1:TRACe4:FEED 'MyMeas3'" 'Pulse settings scpi.parse "SENSe:SWEep:PULSe:MODE PROFILE" scpi.parse "SENSe:SWEep:PULSe:DRIVe 1" scpi.parse "SENSe:SWEep:PULSe:PRF 1" scpi.parse "SENSe:SWEep:PULSe:TIMing 1" scpi.parse "SENSe:SWEep:PULSe:DETectmode 1" scpi.parse "SENSe:SWEep:PULSe:IFBW 1" scpi.parse "SENSe:SWEep:PULSe:MASTer:WIDth 10e-6" scpi.parse "SENSe:SWEep:PULSe:MASTer:PERiod 1e-3"
|