Show Custom Cal Windows during a Guided Calibration


This VBScript program shows how to send commands that allow you to view specific 'custom' windows, and sweep specific channels, during a UI (Cal Wizard) or remote calibration.

The SCPI commands in this example are sent over a COM interface using the SCPIStringParser object. You do NOT need a GPIB connection to run this example.

This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as CalWindow.vbs.  Learn how to setup and run the macro.

These commands are used to show and sweep windows and channels:

See Other SCPI Example Programs

Dim app

Dim scpi

' Create / Get the PNA application.

Set app = CreateObject("AgilentPNA835x.Application")

Set scpi = app.ScpiStringParser

' A comment

'Preset the analyzer

'This creates an S11 measurement in channel 1, window 1

scpi.Execute "SYST:PReset"

' Create and turn on window 2

scpi.Execute "DISPlay:WINDow2:STATE ON"

'Define an S21 measurement in channel 2

scpi.Execute "CALCulate2:PARameter:DEFine:EXT 'MyMeas',S21"

'Associate ("FEED") the measurement name ('MyMeas') to WINDow2

'and give the new TRACe a number (1).

scpi.Execute "DISPlay:WINDow2:TRACe1:FEED 'MyMeas'"

 

'The following lines are all you need in order to:

'show and sweep the custom Cal windows during a UI Calibration

'If sending ONLY these commands, make sure you know the

'correct window and channel numbers to show and sweep.

'Flag windows 1 and 2 to show during Ch1 calibration

scpi.Execute "SENS:CORR:COLL:DISP:WIND1 ON"

scpi.Execute "SENS:CORR:COLL:DISP:WIND2 ON"

'Flag channels 1 and 2 to sweep during Ch1 calibration

scpi.Execute "SENS1:CORR:COLL:SWE:CHAN1 ON"

scpi.Execute "SENS1:CORR:COLL:SWE:CHAN2 ON"

 

' ===========================================================

' The following code performs a remote guided Cal on Ch1.

' From a remote cal, the Cal window does not normally show and sweep

' after the previous standard has been acquired.

' This shows how to include the PACQuire (preview) to view and sweep the Cal Window.

' The Custom window also shows and sweeps due to the flag commands above.

' The flags are cleared at the end of this section.

 

' Specify the DUT connectors

scpi.Execute "sens:corr:coll:guid:conn:port1 ""APC 3.5 female"" "

scpi.Execute "sens:corr:coll:guid:conn:port2 ""APC 3.5 male"" "

' Select the Cal Kit for each port being calibrated.

scpi.Execute "sens:corr:coll:guid:ckit:port1 ""85052D"" "

scpi.Execute "sens:corr:coll:guid:ckit:port2 ""85052D"" "

' Initiate the calibration and query the number of steps

scpi.Execute "sens:corr:coll:guid:init"

numSteps = scpi.Execute("sens:corr:coll:guid:steps?")

MsgBox "Number of steps is " + CStr(numSteps)

' Measure the standards

For i = 1 to numSteps

step = "Step " + CStr(i) + " of " + CStr(numSteps)

strPrompt = scpi.Execute("sens:corr:coll:guid:desc? " + CStr(i))

'send the Preview Acquire command, then prompt

scpi.Execute "sens:corr:coll:guid:PACquire STAN" + CStr(i)

' Do NOT send any Guided Cal commands here or the cal window will not sweep

MsgBox strPrompt, vbOKOnly, step

scpi.Execute "sens:corr:coll:guid:acq STAN" + CStr(i)

Next

' Conclude the calibration

scpi.Execute "sens:corr:coll:guid:save"

MsgBox "Cal is done!"

 

'Remove the Custom Window flags

scpi.Execute "SENS:CORR:COLL:DISP:WIND:AOFF"

'Remove the channel sweep flags

scpi.Execute "SENS:CORR:COLL:SWE:CHAN:AOFF"