|
This 15-pin female D-sub connector allows connection of external VGA monitors. With the following resolution settings, you can simultaneously view the VNA display and a remote monitor. |
||||||||
|
2. Click Start -> Control Panel -> Hardware and Sound -> Display. |
3. Under Multiple displays select Duplicate desktop on 1 and 2. |
4. Click OK, then OK again to confirm. |
The VNA must be set to the default resolution (640 x 480). While on any other resolution setting, only the external monitor can be viewed. To change resolution:
Right-click on the VNA desktop, then click Screen resolution.
Adjust display resolution.