The following process can be used to setup all analyzer measurements:
Step 1. Set Up Measurements
Reset the analyzer, create a measurement state, and adjust the display.
Step 2. Optimize Measurements
Improve measurement accuracy and throughput using techniques and functions.
Step 3. Perform a Measurement Calibration
Reduce the measurement errors by performing a calibration.
Step 4. Analyze Data
Analyze the measurement results using markers, math operations, and limit tests.
Step 5. Print, Save or Recall Data
Save or print the measurement data.