Internal Source Modulation

This feature allows any PNA/PNA-X port to be stimulated by a modulated signal and is supported by all measurement classes (requires Option S93072B and synthesizer 7). Internal source modulation allows any of the internal synthesizers to replace traditional sources. In addition, internal source modulation can be set as a global source.

In this topic:

Modulation Below 3.2 GHz

When using an internal modulated source, the low band source is automatically set from Low Bnd Filtered to Low Bnd Hi Pwr. The Low Bnd Hi Pwr mode has significant low frequency spurious when the carrier is below 3.2 GHz. In this case, the Low Bnd Filtered mode can be used below 3.2 GHz to reduce harmonics. The filtered paths are divided into frequency bands ranging from 10 MHz to 3.2 GHz. Each band indicates a low-pass filter with a cutoff slightly above the highest frequency of the range. The frequency band is determined by the carrier frequency. A carrier offset may be needed to keep the carrier frequency in a correct band while avoiding filtering the multitone signal.

The following table shows the frequency range of each band when using the filtered path.

Band Number

Frequency Range
(MHz)

0

10 - 14

1

14 - 19

2

19 - 27

3

27 - 38

4

38 - 53

5

53 - 75

6

75 - 105

7

105 - 146

8

146 - 205

9

205 - 250

10

250 - 396

11

396 - 500

12

500 - 628

13

628 - 1000

14

1000 - 1500

15

1500 - 2000

16

2000 - 3200

How to Set Up Internal Source Modulation

  1. Press Sweep > Source Control > Global Source.... The Global Source Preferences dialog is displayed:



    If the VNA has a synthesizer version earlier than 7 and does not have the S93072B license, the Modulation column will be grayed out and not available:

  1. Click in the Modulation column corresponding to the VNA port to be modulated then click on the Edit button:.


  2. The Modulation Port X dialog should be displayed as shown below:


  3. Click on the "Load File..." button then load an existing modulation file.

Note: Modulation files can be created using the Create Modulation dialog (*.mdx) in the SA/MOD/MODX measurement classes. Using the Create Modulation dialog to create modulation files allows you to verify the signal before using it.

  1. Check the Enable Modulation box.
  2. The DAC Scaling sets the scaling factor used for the waveform (full scale = 70%). This ensures that the DAC filter does not output a signal that is larger than the DAC's maximum output level, which can cause distortion in the system.
  3. Check Enable Source Correction to enable source correction after a source modulation calibration is performed then click OK.
  4. In the Global Source Preferences dialog, change the State column to ON to turn the source power on.
  5. Change the Global column to ON to set it as a global source. Learn more.