Swap Adapters and Offset Delay Calibration Methods
The Swap Adapters or Offset Delay calibration method is used when you 
 do NOT have calibration standards with the same connector type as your 
 DUT. In this case, the Offset Delay is the preferred calibration method 
 over the Swap Adapters method.
The Swap Adapters calibration method (also known as Swap Equal Adapters 
 and Equal Length Adapters) was used in the past as a quick alternative 
 to the more tedious adapter 
 removal method. This method requires that the adapters be of equal 
 electrical length. There are two adapters for each port. The swap equal 
 adapter method implicitly assumes the adapters have identical return loss. 
 The finite return loss of each adapter on each port degrades both the 
 residual directivity and residual match terms. The offset delay calibration 
 only has one adapter. The return loss of this one adapter will degrade 
 the residual directivity and residual match error terms.
Note:  For 
 any other reason, these calibration methods are NOT 
 recommended because the Unknown 
 Thru method is more convenient AND more accurate.
The Offset Delay calibration method uses the available standards for 
 calibration then adds offset delay to the measurement plane to account 
 for each adapter used. This eliminates the need for adapters with equal 
 electrical length and is preferred over the Swap Adapters method.
Swap 
 Adapters Procedure
The following is an example procedure showing how to perform a Swap 
 Adapters 2-port calibration for a non-insertable DUT. The DUT has 2.92 
 mm connectors. You do NOT have 2.92 mm calibration standards, but you 
 DO have 2.4 mm standards and adapters that have the same electrical delay 
 as the 2.92 mm adapters.
Adapters A1 and A2 = test port to 2.4 mm adapters
Adapters B1 and B2 = test port to 2.92 mm adapters
	
	
	
		| 
			Start the Cal Wizard and select Guided (Smart) 
			 Cal.  Note: The 
			 VNA will NOT prompt you to connect the adapters by name or 
			 when to swap the adapters. | 
	
		| 
			Specify the connector type and gender and 
			 Cal Kit of the adapter that you will be using (2.4 mm) - NOT 
			 the connector type of the DUT (2.92 mm). By specifying the 
			 connector gender, you are also specifying the Thru method 
			 (flush thru for insertable and Unknown Thru for non-insertable.) 
			 For example, when both DUT ports have female connectors, we 
			 will perform an Unknown Thru cal. | 
	
		| 
			When prompted for reflection standards on 
			 port 1, connect the Open, Short, and Load standards to Adapter 
			 A1.When prompted for reflection standards on 
			 port 2, connect the Open, Short, and Load standards to Adapter 
			 A2. | 
 | 
	
		| 
			When prompted for a Thru connection, swap 
			 Adapter A1 and A2 for B1 and B2. Connect the Thru device. 
			 This could be any device that meets the requirements of the 
			 Unknown 
			 Thru standard. In the case of a non-insertable DUT, connect 
			 B1 and B2. | 
 | 
	
		| 
			Make DUT measurements with Adapters B1 and 
			 B2 in place. | 
 | 
 
Offset 
 Delay Procedure
The following is an example procedure showing how to perform a 2-port 
 calibration for a non-insertable DUT using Offset Delay to account for 
 the added delay of two adapters. The DUT has 2.92 mm connectors. You do 
 NOT have 2.92 mm calibration standards, but you DO have 2.4 mm standards 
 and adapters.
Adapters = test port to 2.4 mm (female)-to-2.92 mm (male) adapters
	
	
	
		| 
			Start the Cal Wizard and select Guided (Smart) 
			 Cal. | 
	
		| 
			Specify the connector type and gender and 
			 Cal Kit that you will be using (2.4 mm) - NOT the connector 
			 type of the DUT (2.92 mm). By specifying the connector gender, 
			 you are also specifying the Thru method (flush thru for insertable 
			 and Unknown Thru for non-insertable.) For example, when both 
			 DUT ports have female connectors, we will perform an Unknown 
			 Thru cal. | 
	
		| 
			When prompted for reflection standards on 
			 port 1, connect the Open, Short, and Load standards.When prompted for reflection standards on 
			 port 2, connect the Open, Short, and Load standards. | 
 | 
	
		| 
			When prompted for a Thru connection, connect 
			 the Thru device between port 1 and port 2. This could be any 
			 device that meets the requirements of the Unknown 
			 Thru standard. In this example of a non-insertable DUT, 
			 a female-to-female 2.4 mm barrel adapter is used as the Thru 
			 device. | 
 | 
	
		| 
			Click on Response, Cal, 
			 then select Port Extension. 
			 The Port Extension dialog is used to electrically 
			 move the measurement reference plane after you have performed 
			 a calibration to account for the two adapters. Learn more 
			 about Port Extensions.Select Port 
			 1 and enter the delay of the adapter connected to Port 1.Select Port 2 and 
			 enter the delay of the adapter connected to Port 2.Click OK. | 
 | 
	
		| 
			Make DUT measurements with Adapters and DUT 
			 in place. | 
 |