To access either the downlink or uplink gap editing window:

In the tree view under
Physical, click the gap
you wish to edit.
or
Click Physical to display all previously
added bursts in the right pane. Double-click the first column of the gap
you wish to edit.
Gap Interval [samples]
Use this cell to set the length of the gap in integer units of samples. The maximum gap size depends on the sampling rate, oversample ratio, cyclic prefix, and frame size. When you change Gap Interval [us], this value is automatically recalculated by dividing the specified time by the sample time. The default value is 800.
Gap Interval [us]
Use this cell to set the length of the gap in microseconds. Changing the Gap Interval [samples] value automatically recalculates this value. The default value is 100.
Sample Time [us]
This cell displays the sample time of the OFDM waveform in microseconds. The sampling time depends on the bandwidth that you set in the Project Property window. You cannot edit this cell.