Clicking Instruments
in the tree view displays a table
in the right pane with LAN and GPIB connectivity parameters for up to
ten signal generators. When you download a configuration to multiple signal
generators, the data is downloaded serially, one instrument at a time,
in the order shown in the table. (For more information on connecting to
the signal generator, see Equipment
Setup.)

This column designates the signal generator connection number. The currently selected connection number also appears in the status bar at the bottom of the main window. You cannot edit cells in this column.
The cells in this column set the connectivity state for the Signal Studio
software and the signal generator. A checkmark
indicates that the connection to the signal
generator is active.
The cells in this column report whether or not the connection to the signal generator is valid after testing an active connection. OK or Fail is displayed.
The cells in this column set the connection type. You can choose either LAN or GPIB.
If you are using LAN, you must enter the signal generator's Host Name or IP address in this column for all active connections. The address for the currently selected connection also appears in the status bar at the bottom of the main window.
|
|
The Signal Studio software automatically recalls previously entered IP addresses (or hostnames) for the Host Name or IP cell. If the signal generator's dynamic host configuration protocol (DHCP) is enabled, you must change the IP address in this cell to reflect the new IP address the network may have reassigned to the signal generator when it was last turned on. Since the hostname never changes in DHCP mode, entering it instead of the IP address is a more efficient option. |
If you are using GPIB, you must enter the PC's GPIB board setting in this column for all active connections.
If you are using GPIB, you must enter the signal generator's GPIB address in this column for all active connections.
The cells in this column report additional information about the connectivity of the signal generator and Signal Studio software.

To validate the connection for a specific signal generator, click anywhere
in its row. An indication arrow
moves to the row of the signal generator
you selected. Click Test Connection
and observe the messages in the Result
and Note cells. For help with
error messages, refer to Troubleshooting.

To validate the connections for multiple signal generators, click Test All Connections and observe the messages in the Result and Note cells. For help with error messages, refer to Troubleshooting.