Currently there is no API available with the software to allow access to the waveform configuration capabilities via software control. However, it is being considered for a future release.
|
|
You can configure and generate the waveforms and save them as files on your PC. These files can then be transferred to the signal generator and played back as desired under software control, using the SCPI commands available for the signal generator. The commands are documented in the ESG/PSG SCPI Command Reference or the MXG SCPI Command Reference. |