This table is used for the QPSK bit pattern. The symbol period is the pulse width (100%-100%) divided by the number of symbols. QPSK has two bits per symbol. The symbol mapping is as follows:
00 = 0°
01 = 90°
11 = 180°
10 = 270°
To add steps (index items) to the table:
Right mouse click in the Custom QPSK table or select the Edit menu.
Select
New items
Enter the
number of
steps
for the pattern