Open topic with navigation
The Fall Time parameter is the time taken for the falling edge of the pulse to decrease from 100% to 0% amplitude.
Range is a positive time value
Units are:
s - seconds
ms - milliseconds
us - microseconds
ns - nanoseconds
API units are seconds: s