Generate Correction

Selection of this menu item forces a correction measurement to determine the correction coefficients for the current pattern library settings . The measurement data is stored in the data base and will replace any existing data for the current setup. The signal generator, arbitrary waveform generator, and analyzer must be connected correctly and share a common 10 MHz reference for the measurement to work. The sample clock minimum, maximum, resolution and reset values are system configuration specific: