This read-only field describes the total time duration of an object. The time measurement for a pattern is calculated from the repetition interval for the object type. For example, if a pattern has one pattern item that is 10 us long and is repeated twice then the object length is 20 us.
For Object Types
, the Object Length is the sum of rise time (0-100%), pulse Width (100%-100%), and fall time (100%-0) as defined in the Pulse Library.For Object Types
, the Object Length is the time duration of the pattern.For Object Type
, this field is blank.Units are:
s - seconds
ms - milliseconds
us - microseconds
ns - nanoseconds