API Programming Examples

This section contains information on programming, using the Pulse Building API. Several programming examples that demonstrate how to use the pulse building API using Microsoft Visual Basic 6.0 are given. The Pulse Building API is installed on the computer when the Pulse Building software is downloaded.

Refer to the section on Pulse Building Classes for information on the properties, methods and enumeration types associated with the Pulse Building software. The API members can also be viewed using the Object Browser in Microsoft Visual Basic. It is available from the View menu in the Visual Basic project.

The programming examples, with the exception of the Executive Test example, duplicate the examples manually generated in the Pulse Building Examples section of this Help document. You can run the manual examples and compare the results to the results obtained from the programming example.

The following is a list of the contents for this section: