QPSK (Quadrature Phase Shift Keying)

Each state is offset 90 degrees from adjacent states. Step size is the time duration for each I/Q state (defined as 1/symbol rate).

The following figure shows QPSK phase state changes for a trapezoidal or raised-cosine pulse (Width (100%-100%)).For custom profile and custom I/Q pulses the modulation is applied from the first point of data through to the last point of data.