Staggered Hop Data is an array that contains the staggered frequency hopping interval data used for a Staggered Hop Pattern Type. The following figure shows an example of staggered hop data.
The stagger hops are maintained in a variable length double array. The number of hops is equal to the length of the array. The first value in the array is mapped to Hop Start. See Import.
Changing the Hop Pattern Type resets this property.
|
Units |
Default |
Min |
Max |
|---|---|---|---|
|
Hz |
0 Hz |
0 |
+/- Signal Bandwidth/2* |
* Signal Bandwidth is hardware dependent. The absolute maximum bandwidth is +- 2GHz. This bandwidth can only be achieved with a PSG and option 016 and an M8190A arbitrary waveform generator.