Staggered PRI Data is an array that contains the staggered pulse repetition interval data used for a Staggered PRI Pattern Type. The following figure shows an example of staggered PRI data.
The stagger PRIs are maintained in a variable length double array. The number of pulses is equal to the length of the array. The first value in the array is mapped to PRI Start and Repetition Interval. See Import.
Changing the PRI Pattern Type resets this property.
|
Units |
Default |
Min |
Max |
|---|---|---|---|
|
s |
10.3 us |
0 |
100E6 |