Wobbulation Deviation

Wobbulation Deviation sets the wobbulation deviation for Sawtooth, Sinusoidal, or Triangular PRI Wobbulation impairment. The wobbulation deviation can be a positive or negative value. A positive value causes the pattern to start at zero and increase. A negative value causes the pattern to start at zero and decrease.

Units

Default

Min

Max

s

0 s

–10 ms

10 ms

The following figures show the effect of positive and negative wobbulation deviation. The first figure shows that for a positive deviation, the PRI wobbulation impairment starts at zero and increases. The second figure shows that for a negative deviation, the PRI wobbulation impairment starts at zero and decreases.