Clicking Arbitrary Waveform Generator in the
tree view
provides access to the Arb's instrument controls in the main window. The available parameters vary, depending on the Arb model. This topic describes connection to the M9330A, N8241A, and N6030A. Click the plus
box or
arrow to expand each set of parameters.
The Arbitrary Waveform Generator settings provide direct control of the external Arb. These settings are only available when the system is configured for External I/Q or Wideband I/Q. The values are sent to and from the Arb using the Update to Instrument and Update from Instrument buttons. If Real Time Update is enabled, however, any changes you make are immediately sent to the instrument. Whenever you download or play a waveform, all of the current Arb settings are sent to the instrument.

Press this button to send the software parameters to the connected instrument.

Press this button to retrieve the parameters from the connected instrument.

Press this button to provide a software trigger to the Arb.

Press this button to provide a software trigger to the Arb.