These parameters are overwritten by the application during a download or play.
Range: for specified range values, see the signal generator's data sheet
Enter a value to set the signal generator’s output frequency. Use abbreviations for faster entry (example: 1g = 1.000000000000 GHz).
Range: for specified range values, see the signal generator's data sheet
Enter a value to remotely set the signal generator’s output amplitude.
Double-click or use the drop-down menu to control the signal generator’s RF output state.
Range: –200 GHz to 200 GHz
Enter a value to set the signal generator’s output frequency offset. Use abbreviations for faster entry. For example: 1k = 1.000000000000 kHz.
Range: –200 dB to 200 dB
Enter a value to remotely set the signal generator’s output amplitude offset.
Double-click or use the drop-down menu to turn the signal generator's RF modulation on or off. This function applies to all enabled modulation, including I/Q modulation, pulse modulation, AM and FM modulation.