Create a Noise Power Ratio Signal (NPR)

Follow this procedure to create a noise power ratio signal and to perform these related tasks:

  1. Start the software and configure the hardware.

  2. From the ClosedMode menu, select ClosedNoise Power Ratio (NPR).

  3. Use the default settings or configure the ClosedNPR Settings as desired.

  1. Click to download and play the waveform.

  2. Configure the analyzer to view the signal.

Example NPR Signal

The following figures show an example of the default settings for a ClosedWideband Arb Waveform Generator with Calibration.

  1. Configure the analyzer as follows:

The analyzer display should look similar to the figure below.

 

  1. Change the settings to:

Notice the carrier feedthrough at 10 GHz.

 

 

Return to top

 

Set the NPR Noise Offset

  1. To offset the notch and noise away from the carrier, set the ClosedNoise Offset = 1 MHz.

  2. Click to download and play the waveform.
    Notice that the PSG marker is at 9.999 GHz but the notch itself is still centered around 10 GHz.

 

 

Return to top

 

Set the NPR Corrections

  1. Configure the ClosedNPR Settings as follows:

  1. Click to Download.
    A progress window will appear during the correction process. In this case the correction algorithm may not achieve the 70 dB suppression in all tones.

 

  1. Click   to Play the waveform.

  2. Configure the analyzer:

 

 

Return to top