5. Dual ARB

ARB

Choice: On | Off
Default: Off

Double-click or use the drop-down menu to control the ARB state.

Turning the Arb on also turns on the I/Q and ensures that the Arb output is connected to the I/Q modulator.

This parameter is overwritten by the application during a download or play.

ARB Sample Clock

Range: for specified range values, see the signal generator's data sheet

Enter a value to set the signal generator’s sample clock frequency. Use abbreviations for faster entry (example: 1m = 1.000000 MHz).

This parameter is overwritten by the application during a download or play.

VCO Clock

Choice: Internal | External
Default: Internal

Double-click or use the drop-down menu to select the signal generator’s VCO Clock. The software does not control the instrument providing the external sample clock.

The external VCO Clock is only available if the signal generator is an ESG or PSG model with option HEC for external clock support. See the signal generator’s user’s guide for information on VCO Clock.

This parameter is overwritten by the application during a download or play.

Waveform Runtime Scaling

Range: 1%−100%
Default: 70%

Use this parameter after downloading and synchronizing with the signal generator.

Set or change the Waveform Runtime Scaling to reduce the overshoot associated with the digital-to-analog convertor (DAC) interpolation filter. Enter a scaling value for the signal generator to apply to the waveform while it is playing. Use scaling to get the best dynamic range without overflowing the I and Q digital to analog converters. At 100 percent, some overshoot may occur; therefore the default setting is 85 percent.

This parameter is available for all systems configured with an internal Arb.

I/Q Modulation Filter

Choice: Auto | 2.1 MHz | 40 MHz | Through
Default: Auto

Use this parameter after downloading and synchronizing with the signal generator.

Double-click or use the drop-down menu to select a filter for I/Q signals modulated onto the RF carrier. The bandwidth of the baseband signal should dictate the minimum reconstruction filter bandwidth you choose. Depending on the oversampling ratio and where the image frequencies appear, you may want to select a wider bandwidth.

This parameter is not available with all instrument model numbers and may be grayed out.

This parameter is overwritten by the application during a download or play.

I/Q Output Filter

Choice: Auto | 40 MHz | Through
Default: Auto

Use this parameter after downloading and synchronizing with the signal generator.

Double-click or use the drop-down menu to select a filter or through path for routing I and Q signals to the rear panel I/Q outputs.

This parameter is not available with all instrument model numbers and may be grayed out.

Modulation Attenuation Mode

Choice: Auto | Manual
Default: Auto

Use this parameter after downloading and synchronizing with the signal generator.

Double-click or use the drop-down menu to select the mode of the internal I/Q modulator.

This parameter is not available with all instrument model numbers and may be grayed out.

Modulation Attenuation

Range: 0.00−40.00 dB
Default: 10.00 dB

Set Modulation Attenuation Mode to Manual to enable this parameter.

Set the attenuation of the I/Q signals being modulated through the signal generator RF path. Adjusting the attenuation may reduce signal distortion and improve the overall dynamic range.

When ALC is enabled, the RF output amplitude will not change while the attenuator value is changed until the ALC range is exceeded.

High Crest Mode

Choice: On | Off
Default: Off

Use this parameter after downloading and synchronizing with the signal generator.

Double-click or use the drop-down menu to enable or disable the signal generator’s high crest mode.

This parameter is not available with all instrument model numbers and may be grayed out.

ARB Reference

Choice: Internal | External
Default: Internal

Use this parameter after downloading and synchronizing with the signal generator.

Double-click or use the drop-down menu to select the signal generator’s ARB reference source.

This parameter is not available with all instrument model numbers and may be grayed out.

This parameter is overwritten by the application during a download or play.

Reference Frequency

Range: 0.2500000–100.0000000 MHz
Default: 10.0000000 MHz

Set ARB Reference to External to enable this parameter.

Use this parameter after downloading and synchronizing with the signal generator.

Enter the frequency value of the external reference when using an externally supplied reference signal. See the signal generator’s user’s guide for information on external references.

This parameter is not available with all instrument model numbers and may be grayed out.