Double-click or use the drop-down menu to select the M8190A trigger source.
Internal - Use the internal trigger source. Be sure to set the trigger frequency.
External - Use the trigger provided to the TRIGGER IN input on the M8190A front panel. Be sure to set the trigger threshold, polarity and impedance.
Range: 0.1 Hz to 30 MHz
Set the internal trigger frequency. Use abbreviations for faster entry (example: 1m = 1.000000 MHz).
Range: -5.0 V to 5.0 V
Set the external trigger threshold. Use abbreviations for faster entry (example: 50m = 50 mV).
Double-click or use the drop-down menu to select the M8190A trigger polarity.
Positive - Trigger on the positive going edges of the signal.
Negative - Trigger on the negative going edges of the signal.
Either - Trigger on the positive or the negative going edges of the signal.
Double-click or use the drop-down menu to select the M8190A trigger impedance.
Low-50 Ohm - Set the trigger input impedance to 50 Ohms.
High-1K Ohm - Set the trigger input impedance to 1000 Ohms.
Double-click or use the drop-down menu to select the M8190A event source.
External - Use the trigger provided to the EVENT IN connector on the M8190A front panel. Be sure to set the event threshold, polarity and impedance.
Trigger - Use the specified trigger signal for the event.
Range: -5.0 V to 5.0 V
Set the external event threshold. Use abbreviations for faster entry (example: 50m = 50 mV).
Double-click or use the drop-down menu to select the M8190A event polarity.
Positive - Trigger on the positive going edges of the signal.
Negative - Trigger on the negative going edges of the signal.
Either - Trigger on the positive or the negative going edges of the signal.
Double-click or use the drop-down menu to select the M8190A event impedance.
Low-50 Ohm - Set the event input impedance to 50 Ohms.
High-1K Ohm - Set the event input impedance to 1000 Ohms.
Accesses the properties for this channel. The properties for channel 1 and channel 2 are identical.
Range: 0.0 V to 1.5 V
Set the sync marker output amplitude. Use abbreviations for faster entry (example: 50m = 50 mV).
Range: -250 mV to 1.5 V
Set the sync marker amplitude offset. Use abbreviations for faster entry (example: 50m = 50 mV).
Range: 0.0 V to 1.5 V
Set the sample marker output amplitude. Use abbreviations for faster entry (example: 50m = 50 mV).
Range: -250 mV to 1.5 V
Set the sampler marker amplitude offset. Use abbreviations for faster entry (example: 50m = 50 mV).