Clicking Quick Setups in the
tree view
displays the setup buttons in the right pane that enable you to choose
between using simulated hardware, a saved Quick Setup, or saving the current
configuration as a Quick Setup.
Selecting a Quick Setup displays the system details for that configuration.
Saves the current application state as a quick setup. Enter a name for
your setup in the
window
that appears.
All hardware parameters from the Signal Generator and Arbitrary Waveform Generator nodes are saved. The file saving location and extension are automatically added to the user-defined file name.
Opens an existing application quick setup file. The quick setup file contains both the application settings as well as the hardware configuration. When a quick setup file is loaded, the hardware information contained in the file is used to configure the system.
The hardware settings may not match those currently shown in the Instrument Controls window of the Signal Generator or the Arbitrary Waveform Generator nodes. Use Update to Instrument to synchronize the hardware parameters, if desired.
Deletes the selected quick setup from the list. Confirm or cancel the
deletion in the
window
that appears.
Allows you to change the name of the selected quick setup file.