A Vector Signal Generator is used to generate a repetitive signal with a given CCDF (Complementary-Cumulative-Distribution-Function) and PSD (Power Spectral Density).
The following diagram shows a typical hardware setup using an N5182B MXG with the signal connected to the VNA rear-panel Port 1 J10 input connector.
Note: Though the following setup example uses an N5182B MXG, an M8190A with E8267D PSG, or an M9383A MCS can also be used as the external source.

The following diagram shows a typical high power hardware setup using an M8190A with E8267D PSG with the signal connected to the VNA rear-panel Port 1 J10 input connector.