Displaying Phase Noise Parameters

Trace Measurement Parameters

How to select and configure Measurement Parameters

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Trace > Trace Setup >  Measure....

  2. Select a parameter.

  1. Click Instrument.

  2. Select Trace.

  3. Select Measure....

  4. Select a parameter

 

Measure Dialog help

Programming Commands

 

PN_b2 - Integrated phase noise measured at VNA input b2 (Test Port Receiver 2).

AM_b2 - Amplitude modulation measured at VNA input b2 (Test Port Receiver 2). This parameter measures the percentage of the modulation of the carrier.

Note: The VNA input receiver number can be changed using the VNA Input function in the RF Path tab or by pressing Meas > Main> VNA Input.

New Trace - Add a new trace.

Channel N - Select a channel number for the new modulation distortion trace.

Window N - Select to create the new trace in an existing window or new window.

Select All - Select all measurement parameters.