The following VB Script example exercises the COM commands used to control the Z5623AK64 testset.
For a description of each command, see TestsetControl Object
See Other COM Example Programs
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save on the VNA hard drive as Testset.vbs. Learn how to setup and run the macro.
|
' Demonstrate some COM commands for external testsets. Dim pna Set pna = CreateObject("AgilentPNA835x.Application") Sub DemoTestset(na) Dim testsets, tset1 Dim portNum Dim chNum, address Set testsets = na.ExternalTestsets chNum = 1
' Load a configuration file. ' NOTE: the K64 testset is only compatible with 4-port analyzers. address = 0 testsets.Add "Z5623AK64", address
' Get the testset object ' in the testsets collection. Set tset1 = testsets(1)
' Show the selections available for each port. For portNum = 1 To 4 MsgBox("Port " & CStr(portNum) & " catalog: " & tset1.PortCatalog(portNum)) Next
' Set port mappings on channel 1. tset1.OutputPorts(chNum) = "5 ext R,2 int R,3 int R,6 int R"
' Set control lines. tset1.ControlLines(chNum) = 85
' Set label. tset1.Label(chNum) = "Some label"
' Enable external testset control. This automatically enables status bar display as well. tset1.Enabled = True End Sub ' The testset used in this demo is only usable on 4-port analyzers If (pna.NumberOfPorts <> 4) Then MsgBox("This program only runs on 4-port analyzers.") Else DemoTestset(pna) End If |