The following VB Script example exercises the COM commands used to set up the Power Range feature to access data sheet specified and typical max and min power levels (in dBm). Max power refers to the maximum leveled source power.
This VBScript (*.vbs) program can be run as a macro in the VNA. To do this, copy the following code into a text editor file such as Notepad and save it on the VNA hard drive as RxLevel.vbs. Learn how to setup and run the macro.
|
Set Application = CreateObject("AgilentPNA835x.Application", "A-N5242A-90065") Set PowerRange = application.Capabilities.PowerRange powerRange.Reset powerRange.PortNumber = 1 powerRange.PathElement("Src2Out1LowBand").Value = "HiPwr" powerRange.RangeStartFrequency = 1e9 powerRange.RangeStopFrequency = 10e9 maxPower = powerRange.RangeGetMaxPower minPower = powerRange.RangeGetMinPower
MsgBox("Max power: " & maxPower & " dBm" & Chr(10) &_ "Min power: " & minPower & " dBm" ) End Function |
|
Set Application = CreateObject("AgilentPNA835x.Application", "A-N5242A-90065") Set PowerRange = application.Capabilities.PowerRange powerRange.Reset powerRange.PortNumber = 3 powerRange.PathElement("Src2Out1LowBand").Value = "HiPwr" powerRange.DiscreteFrequencies = Array(1e9,2e9,3e9,4e9) maxPower = powerRange.DiscreteGetMaxPowerArray minPower = powerRange.DiscreteGetMinPowerArray
MsgBox( "Frequency: " & ArrayToString(powerRange.DiscreteFrequencies) & " Hz" & _ Chr(10) & "Max power: " & ArrayToString(maxPower) & " dBm" & Chr(10) &_ "Min power: " & ArrayToString(minPower) & " dBm" )
Function ArrayToString(Arr) ArrayToString = "[" If IsArray(Arr) Then ArrayToString = ArrayToString & CStr(Arr(0)) For i = 1 to ubound(Arr) ArrayToString = ArrayToString & "," & CStr(Arr(i)) Next End If ArrayToString = ArrayToString & "]" End Function |