Description |
Triggered by a calibration event. See a list of CAL Events. Note: Some Severe Events are also used as Error Messages |
VB Syntax |
Sub app_OnCalEvent(ByVal eventID As Variant, ByVal chanNum As Variant, ByVal measNum As Variant) |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
eventID |
Code number of the event which occurred |
|
chanNum |
Channel Number of the event |
|
measNum |
Measurement Number of the event |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
Sub pna_OnCalEvent(ByVal eventID As Variant, ByVal channelNumber As Variant, ByVal measurementNumber As Variant) |
|
|
|
C++ Syntax |
HRESULT OnCalEvent(VARIANT eventID, VARIANT channelNumber, VARIANT measurementNumber) |
Interface |
IApplication |
512 naEventID_CAL_QUESTIONABLE
514 naEventID_CAL_STATE_NOT_HW_COMPATIBLE
516 naEventID_CAL_CORRECTION_TURNED_OFF
517 naEventID_CAL_CORRECTION_TURNED_OFF_INTERPOLATION_OFF
518 naEventID_CAL_CORRECTION_RESTORED
519 naEventID_CAL_CORRECTION_TURNED_OFF_FREQRANGE_EXCEEDED
520 naEventID_CAL_CALTYPE_SET_TO_NONE
521 naEventID_CAL_CORRECTION_TURNED_OFF_NOT_AN_SPARAM
524 naEventID_SOURCE_POWER_CAL_COMPLETED
592 naEventID_SOURCE_POWER_CAL_NOT_PRESENT
593 naEventID_SOURCE_POWER_CAL_NOT_COMPLETE
594 naEventID_SOURCE_POWER_CAL_REMOVE_TRACE
595 naEventID_SOURCE_POWER_CAL_REMOVE_MEAS
596 naEventID_SOURCE_POWER_CAL_POWER_CHANGED
598 naEventID_INSUFFICIENT_SLIDE_MOVEMENT
613 naEventID_CALSET_NOT_FOUND
617 naEventID_CALSET_FILE_NOT_VALID
634 naEventID_CALSET_LOAD_FAILED
635 naEventID_CALSET_SAVE_FAILED
637 naEventID_CALSET_FILE_NOT_COMPATIBLE
639 naEventID_NEW_CALSET_FILE_CREATED
644 naEventID_CAL_COULD_NOT_TURN_ON
693 naEventID_ERROR_FIXTURING_S2PFILE_CANNOT_OPEN
696 naEventID_ERROR_FIXTURING_TURNED_OFF
701 naEventID_MORE_THRU_PATHS_NEEDED
Errors and the SCPIStringParser Object