Description |
Triggered by a system event. See a list of System Events, also known as general events. See also EnableSourceUnleveledEvents Property Note: Some Severe Events are also used as Error Messages |
VB Syntax |
Sub app_OnSystemEvent(ByVal eventID As Variant) |
|
|
|
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
eventID |
Code number of the event which occurred |
|
chanNum |
Channel Number of the event |
Return Type |
Not Applicable |
Default |
Not Applicable |
|
|
|
Examples |
Private Sub pna_OnSystemEvent(ByVal eventID As Variant) |
|
|
|
C++ Syntax |
HRESULT OnSystemEvent(VARIANT eventID) |
Interface |
IApplication |
2048 naEventID_OPTION_NOT_INSTALLED
2049 naEventID_FEATURE_NOT_AVAILABLE
2050 naEventID_FEATURE_NOT_VALID
2063 naEventID_RECALLFILE_SUCCESS
2130 naEventID_PRINTER_TROUBLE
2144 naEventID_NO_LICENSE
2163 naEventID_PRESET
Errors and the SCPIStringParser Object