Write-only |
About Segment Sweep |
Description |
Adds segments to the Segments collection, but does not turn the segments ON. |
VB Syntax |
segs.Add (item, [size]) |
|
segs |
A segments collection (object) |
|
item |
(variant) Number of the new segment. If it already exists, a new segment is inserted at the requested position. |
|
size |
(long integer) Optional argument. The number of segments to add, starting with item. If unspecified, value is set to 1. |
Return Type |
None |
Default |
None |
Examples |
Segs.Add 1, 4 'Adds segments 1,2,3,and 4. (does NOT automatically turn segments ON) |
C++ Syntax |
HRESULT Add(VARIANT index, long size); |
Interface |
ISegments |
Remarks |
To ensure predictable results, it is best to remove all segments before defining a segment list. For each segment in the collection, do a seg.Remove. |