Write-only |
About Analyzer Events |
Description |
Sets event filtering to monitor all events in the analyzer. This is the default setting when subscribing to events. This could slow the measurement speed of the analyzer significantly. |
VB Syntax |
app.AllowAllEvents |
Variable |
(Type) - Description |
|
app |
An Application (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.AllowAllEvents |
C++ Syntax |
HRESULT AllowAllEvents() |
Interface |
IApplication |