Write-only |
About Performing a Calibration |
Description |
This method is the final call in a calibration process. It calculates error-correction terms, turns error-correction ON and saves the error-correction terms to the channel’s Cal Register or a User Cal Set. Do NOT use this command during an ECAL. Note: The destination (Cal Register or User Cal Set) is determined by the setting of the RemoteCalStoragePreference property. |
VB Syntax |
cal.CalculateErrorCoeffiecients |
Variable |
(Type) - Description |
|
cal |
Calibrator (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
Cal.CalculateErrorCoeffiecients |
C++ Syntax |
HRESULT CalculateErrorCoefficients() |
Interface |
ICalibrator |